2020-03-30 3:16 PM
Hi everybody,
I have installed STM32CUBEMX and also pack for F1 series(V 1.8).
When i generate code for keil or truestudio i expect to have :
#include "main.h"
#include "stm32f1xx_hal1.h"
inside of main.c file but unfortunately it does not generate #include "stm32f1xx_hal1.h".
It is also the same situation with STM32CUBEIDE.
Where is the problem.
Thanks in advance
2020-03-31 12:39 AM
Hello @AAhma.3 ,
The #include "main.h" , which contain the #include "stm32f1xx_hal.h" , is called in the main.c file .
Best Regards,
Khouloud
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.