STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1759 Views
  • 0 replies
  • 2 kudos

VREFBUF not working on STM32H743?

The current STM32CubeMX package cannot generate proper code to initialize the VREFBUF in STM32H743 MCU. Modifications to HAL_MspInit() in stm32h7xx_hal_msp.c can fix this: Add "__HAL_RCC_VREF_CLK_ENABLE();" to user code section 0.In user code sectio...

FLiu.11 by Associate II
  • 1227 Views
  • 1 replies
  • 1 kudos

STM32CubeMX 5.6.1 STM32G4 OPAMP/ PGA configuration issue?

Hello,Fully new with OPAMP, configuration, I made some tries, and for me ther is an issue on the CubeMX code generator. If I want use an OPAMP with PGA with positive gain, I only need non inverting input and output. There is no way to specify this co...

SDMMC fixed

I already reported this bug up at previous versions of the STM32H7 firmware.Now I'm using STM32CubeMX 5.6.1STM32CubeIDE 1.3.1 (arm-none-eabi-gcc 7.3.1)STM32Cube FW_H7 V1.7.0For those who find SDMMC not working, there still is an obvious bug , the way...

Jack3 by Senior III
  • 5125 Views
  • 10 replies
  • 1 kudos

Anyone got STM32H7XX + I2S full-duplex master working?

I have tried to use STM32CubeMX and STM32CubeIDE to generate code. But in CubeIDE I can't create a SPI2_RX DMA Request. And in CubeMX I can't generate a Master Clock Output.So I wonder if there is any handcrafted code anyone written to get this worki...

DViks.1 by Associate II
  • 3175 Views
  • 6 replies
  • 0 kudos

STM32CubeMX 5.6.0 released

What is new in STM32CubeMX V5.6.0? • Added the support of new part numbers in the STM32L0 Series: STM32L071C(B-Z)Ux, STM32L081CZUx, STM32L072C(B-Z)Ux, STM32L082CZUx, STM32L073C(B-Z)Ux, STM32L083CZUx, and STM32L073CZUx • Added the support of the new 8...

FSMC with NAND interface signalling

Hello, I am using STM32L4R9AI (attached the reference manual) with 128GB NAND flash (MT29F128G08CFABBWP-12IT:B TR) (attached its datasheet).1- This is 8bit NAND flash and according to page 104 in the reference manual the last signal is NWAIT/INT whic...

Bug Report on Code Generation for NUCLEO-G474RE

Not a big bug but I wanted to mention it as it tripped me up.I am using STM32CubeMX 5.6.1 with IDE System Workbench 2.9.1I have found that when I setup SPI DMA synchronization the request number doesn't change from 1 when I generate the code or save,...

CH1 by Associate II
  • 2385 Views
  • 4 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.