STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1757 Views
  • 0 replies
  • 2 kudos

AD9833 Module Control

Hello,I want to control the ad9833 module with the stm32f4 development board. I have a library but I couldn't get SPI communication. I cannot get any wave output from the module. I cannot adjust frequency. where can the problem be? I need to create t...

BTaşk.1 by Associate II
  • 5084 Views
  • 5 replies
  • 0 kudos

Resolved! Prescaler and period values for PWM in STM32

I am using STM32F103C8Tx and I am trying to create a PID adjustable PWM. In PID I will be giving values to PWM from 0 to 100 to set the duty cycle. That means my counter period needs to be 100 in Cubemx. Because as I have learnt while I am changing t...

GunkutA by Senior
  • 13921 Views
  • 17 replies
  • 0 kudos

STM32H745ZI-Q Nucleo Ethernet is not working.

Hi,I have STM32H745ZI-Q Nucleo board. I have generated code using STM32CubeMX firmware version H7 1.5.0 (SW4STM32). I have enabled the LwIP Netconn and Ethernet for M7 core in STM32CubeMX. The issue is that it doesn't assign the IP address using DHCP...

I have an issue with ADC and Vrefint

Hi,I working with an STM32L010 controller. I have a confusing issue with one of ADC channel.Here is the configuration:I using ADC channels 1, 3, 6 and Vrefint.Here is the ADC configuration:I forgot the clock configuration:My problem is while the volt...

0693W000001pPovQAE.png 0693W000001pPpKQAU.png 0693W000001pPvNQAU.png
anagy9 by Associate II
  • 1524 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.