2020-05-22 5:49 AM
Today cubemx deleted my repository. I launched it after about two weeks. Is it a bug or some cubemx function?
2020-05-22 5:57 AM
Repositories are stored in:
C:\Users\%USERNAME%\STM32Cube\Repository
See if it's there. If not, you'll probably have to redownload.
No, I can't see CubeMX deleting repositories as a feature. Maybe it just doesn't see them.
2020-05-22 6:02 AM
The folder in the repository path is empty. The folder was not empty at the beginning of the week.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.