STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1757 Views
  • 0 replies
  • 2 kudos

Resolved! Cannot enable IGMP in STM32CubeIDE.

I am using a a very recent version of STM32CubeIDE (Version: 1.3.1) and STM32CubeMX (5.6.1.202004052303). I created a new project for the Nucleo-F207ZG board.I have enabled LWIP and then enabled UDP but the "IGMP module" has no "enabled" option. Is t...

Resolved! STM32F407 EXTI on PI10 not working

Hi guys, I want to use 10 external interrupts. 9 of them are working fine, but one of it makes trouble. I'm using CubeMX and configured the 10 pins as external interupt with falling edge detection and enabled the interrupts. The pins are: PB6, PB7, P...

user 143 by Associate III
  • 2585 Views
  • 5 replies
  • 0 kudos

Resolved! STM32F407 + Freertos + USB VCP + USART IRQ

Hello, I am triying to use the STM32F407 with Freertos ,USB VCP and USART interrupts. My problem is when I include USART interrupts with Freertos, the interrupt is always running. I did other project without the Freertos and everything is OK. I lea...

Asarm.1 by Associate
  • 1366 Views
  • 1 replies
  • 0 kudos

A note on patching internal templates during code generation

Lately I got stuck at a particular issue in STMCubeMX / STM32CubeIDE Device configuration tool, where a certain portion of the HAL library configuration was fixed and overwritten during code generation, more info here.---This above issue has been fix...

0693W000001qBrOQAU.png 0693W000001qBqaQAE.png 0693W000001qBqfQAE.png
TPeča.1 by Associate II
  • 2912 Views
  • 2 replies
  • 1 kudos

[FYI] STM32CubeMX on Raspberry Pi

FYI: To run the cube on raspberry:Download and install Oracle java 1.8.0, arm32 hard float cd /opt; tar xvf jdk-8u251-linux-arm32-vfp-hflt.tar.gzDownload and unzip STM32CubeMXunzip en.stm32cubemx_v5-6-1.zipStart installer/opt/jdk1.8.0_251/bin/java -j...

koendv by Associate III
  • 2853 Views
  • 2 replies
  • 0 kudos

Resolved! Timer not working as expected

Hi,I want to measure time between two events. The events come in as ext- interrupts. I set up a timer like this:TIM_MasterConfigTypeDef sMasterConfig = {0};   /* USER CODE BEGIN TIM6_Init 1 */   /* USER CODE END TIM6_Init 1 */ htim6.Instance = ...

SSchu.4 by Associate II
  • 3486 Views
  • 3 replies
  • 0 kudos

Orange Pin on PB3 DEBUG JTDO-SW0 on chip stm32h753bitx

Hi, I have 3 SAI ports and 2 x SD cards ( FATFS in cubeMX does't set up 2 cards )the chip is supposed to have 4 SAI ports  stm32h753bit6I get conflict errors if;I have asynchronous set on SAI1 A without error on SWD pinI have SDMMC2 in 4 bit mode wit...

benyBoy by Associate II
  • 3580 Views
  • 3 replies
  • 0 kudos

Bug Report : CubeMX 5.6.1 Code Generation STM32L5 HAL_SD_MspInit

Hi,I'm using CubeIDE 1.3.1 with CubeMX 5.6.1, target is a STM32L5 with SDMMC.I had a problem during SD initialisation, which gave me a timeout error every time from SDMMC_CmdGoIdleState call in SD_PowerON.I finally found the problem : the function HA...

OE1 by Associate II
  • 1987 Views
  • 3 replies
  • 1 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.