STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1757 Views
  • 0 replies
  • 2 kudos

Cube MX does not create a project

it does not create a project. I used this ioc file on a working computer,There it earned. How to fix my cube mx? or reinstall Keil 5? I need help. I add Keil project

AArt.1 by Associate II
  • 3105 Views
  • 3 replies
  • 0 kudos

makefile:43 error pls help

Hi!I am trying to create a very first Hello World project like that:/** ****************************************************************************** * @file      : main.c * @author     : Auto-generated by STM32CubeIDE * @brief     : Main program bo...

M.umit by Associate II
  • 2914 Views
  • 4 replies
  • 0 kudos

Debug problems with STM32CubeIDE

Hi,I have a NUCLEO F103RB board with STM32F103RB MCU. I am doing my first program for blinking a LED (I am starting with STM32 MCU family). I use STM32CubeIDE just downloaded in the last days.I compile my simple program without problems.The debug pha...

MSand.1 by Associate II
  • 2404 Views
  • 1 replies
  • 0 kudos

FatFS f_open always returns FR_DISK_ERR on USB stick

Hello, I try to implement some kind of data logger which saves values on an usb stick. The board is based on an STM32F767ZGT6.To do things properly, I have created a fresh new project with STM32CubeMX ( to include later in my main project). Here is w...

Geo En by Associate III
  • 4716 Views
  • 5 replies
  • 2 kudos

Stm32 h7

hi I wanted to ask regarding stm32h7 as I have two main available one for m4 main and the other for m7 main, if I process a variable in the cortex m4 how can I transfer it to the m7?Can i use mdma or dma.....Tanks​

SDall by Associate II
  • 2300 Views
  • 4 replies
  • 0 kudos

Java.lang.NullPointerException occurs during MX script.

CubeIDE 1.2.0 I have a simple script to test the command line setup. The script is loading the .ioc and creating .csv of the pinout. I get partially through the csv command where Java runs into a NullPointerException seen below2020-06-09 12:53:23,629...

PLane.1 by Associate II
  • 1425 Views
  • 2 replies
  • 0 kudos

STM32F303 CubeMX - LL_GPIO_TogglePin() - race condition?

__STATIC_INLINE void LL_GPIO_TogglePin(GPIO_TypeDef *GPIOx, uint32_t PinMask) { WRITE_REG(GPIOx->ODR, READ_REG(GPIOx->ODR) ^ PinMask); }I was trying out a Nucleo F303RE board and installed CubeIDE and the HAL/LL library, then stumbled upon this.Tha...

SKled.1 by Senior II
  • 2717 Views
  • 4 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.