STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1757 Views
  • 0 replies
  • 2 kudos

Backup registers are cleared on reset - STM32G474

Hi all,I have a STM32G474 and data in backup registers (eg. LL_RTC_BKP_DR0) are cleared after reset or power cycle (3.3 V battery is present!).Code is generated by CubeMX with LL drivers. I enabled RTC and disabled all tampers.In the main code, I can...

Martin294 by Associate III
  • 3432 Views
  • 5 replies
  • 2 kudos

Why doesn't the ADC work when I select the prescaler ratio "HRTIM Clock Multiplied by 32" for the timer that triggers the ADC?

HelloI use a HRTIM timer (Timer B) to trigger the ADC (ADC2_IN5) internally (STM32G4).I want to increas the high-resolution clock frequency fHRCK with a prescaler ratio: 170MHz*32=5.44GHz to trigger the ADC via a compare value of 54.400.Unfortunately...

MOys.1 by Associate II
  • 1885 Views
  • 4 replies
  • 0 kudos

Resolved! ADC max clock for STM32H7(47) is wrong

Hello,STM32CubeIDE  1.5.1, latest H7 package for STM32Cube.I have STM32H747-DISC1 board, and STM32CubeMX (in IDE) let me pick max. 36 MHz clock.According to the datasheet STM32H747xI/G datasheet, ADC clock frequency get up to 50 MHz. I overriden freq...

0693W000007CsutQAC.jpg

Resolved! STM32F072RB compatible MCU's in ST

Hi,Is there any pin-to-pin compatible controller available with STM32F072RBTx MCU in ST. Compatible controllers can be with Higher FLASH & RAM size.

LRPS_92 by Associate II
  • 1799 Views
  • 2 replies
  • 0 kudos

Malloc returns NULL Pointer in FreeRTOS task.

Hello Community, I'm using an ST Nucleo-F767ZI and I create my project, for Atollic True Studio, with Cube32MX.In my project I included FreeRTOS v10.I'm in troubled with the malloc function, because this function return a NULL pointer.I have several ...

FedeRico1 by Associate II
  • 11990 Views
  • 14 replies
  • 1 kudos

Bug: STM32CubeMX code generation for STM32cubeIDE

Hello, I have some problem with the latest version of cubeMX (v6.1.1), it won't create a project file for STM32 (well I would like to use simulink with mat/target before using STM32cubeIDE that's why I use cubeMx and the project work with µvision),th...

0693W000007CqeeQAC.png
SDeha.1 by Associate
  • 1998 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.