STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1756 Views
  • 0 replies
  • 2 kudos

Resolved! Unable to compile generated project

Hello all,I am having severe issues trying to compile and getting to work a blink LED example on Simulink using the STM32-MAT/Target version 5.6.At first, I was trying the example on the hands on documentation of the STM32-MAT/Target. Which is blinki...

HTeno.1 by Associate II
  • 8429 Views
  • 7 replies
  • 0 kudos

Resolved! STM32CubeMX eMMC FatFS Support

I would like to get an clear answer about how I can support an eMMC Flash with FatFS on an STM32 (F4xx, F7xx, H7xx).It seems that STM32CubeMX doesn't want to generate a driver when the SDMMC controller is configured in MMC mode.Maybe there is another...

cniclaes by Associate II
  • 2876 Views
  • 5 replies
  • 0 kudos

SDIO,SD1bit,UART4 Disable.

​I want to use uart4_tx and sdio at the same time.But, in cubemx(6.2.1),SDIO->Mode: SD 1 bitUART4->Mode: only Disable.​

MShao.1 by Associate III
  • 4545 Views
  • 10 replies
  • 0 kudos

STM32CubeID V1.6.1 horrible performance

Hi,The actual version of STMCubeIDE has a horrible performance bug, when I change any IP in the MX view. When I change something, it needs min 30 seconds up to 90 seconds A simple activation of CRC IP needs ~35 seconds. This happens with 2 different ...

Osto by Senior
  • 3702 Views
  • 9 replies
  • 1 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.