STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1756 Views
  • 0 replies
  • 2 kudos

STM32H7 SDMMC1 / FatFs / MDMA Not working

Hello,does anyone have experience with using SDMMC1 (1 bit-mode) and FatFs with enabled dma template on a STM32H730VBTx controller?Without dma template I got it working (but it is requiered for FreeRtos)I am using CubeMx in Version 6.1.1Sorry, I am n...

MBrön.1 by Associate
  • 3782 Views
  • 6 replies
  • 1 kudos

F3 Discovery Analog not configuring DMA correctly

I am trying tio use DMA on 3 different channels under DMA. The cube configurator seems to be incorrecta) It does not see that an ADC is configured and make it greenb) The code produced does not clear the DMA Half Complete interrupt c) The IDE configu...

shorai by Associate III
  • 1105 Views
  • 0 replies
  • 0 kudos

I cannot find a program example (HAL_TIM_IC_CaptureCallback() for the input capture mode described in 14.3.6 PWM input mode (13902_STM32_ReferenceManual_11.pdf ). The attached user code works as I expect, but it is unclear to me if everything is correct.

volatile uint32_t udwIC1_Val1 = 0;volatile uint32_t udwIC2_Val1 = 0;volatile uint16_t uwDuty_Cycle = 0;void HAL_TIM_IC_CaptureCallback(TIM_HandleTypeDef* htim){ if (htim->Channel == HAL_TIM_ACTIVE_CHANNEL_1) { udwIC1_Val1 = htim->Instance->CCR1; udwI...

0693W00000APLUMQA5.jpg
RGünt.1 by Associate II
  • 1691 Views
  • 2 replies
  • 0 kudos

Inverting UART TX Pin in STM32F103

Hello,I'm porting code from STM32F072 to STM32F103. In F0 I had a option in CubeMX to invert UART Tx pin polarity and it worked very well. I do not have this option in F103's. Is there any way to invert polarity in this uC?BR, Daniel

DKarc by Associate II
  • 5392 Views
  • 2 replies
  • 0 kudos

Nucleo-H753ZI BUG in default configuration

TM32Cube ver 1.6.1 MX ver 6.2.1 with STM32Cube_FW_H7_V1.9.0 - select Nucleo-H753ZI with default configuration and generate new project - add some activity like HAL_GPIO_WritePin(GPIOB, LD3_Pin, GPIO_PIN_SET); HAL_Delay(1000); HAL_GPIO_WritePin(GPIOB,...

mbarg.1 by Lead
  • 2605 Views
  • 6 replies
  • 0 kudos

Which IDE you would choose from STM32CubeMX supported list?

As we know STM32CubeMX support multiple IDEs:STM32 Cube IDEIARKeilI am in midst to decide which one to use. I find this is crucial decision as this would be one used throughout development till production and I don't want to waste time due to toolcha...

BParh.1 by Senior III
  • 2851 Views
  • 2 replies
  • 2 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.