STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1756 Views
  • 0 replies
  • 2 kudos

STM32 CUBEMX v6.3.0 does not work with H7 firmware v1.8

I recently upgraded CubeMX to latest v6.3.0 and I have my project based on STM32H743IIT6 microcontroller. If I try to open my project which is made using H7 firmware v1.8 without migrating it to latest v1.9 then CubeMX gets hanged and its not able t...

VShet.2 by Associate III
  • 2096 Views
  • 3 replies
  • 0 kudos

Resolved! Hi I am concerned about the following microcontroller : STM32H753XIH6TR When using cube Mx to configure the timers on pin PA1_C the options specified in the data sheet are not avaliable. How do I access these functions?

Please see attatched image of functions specified in datasheet.Please see image attatched of functions avalailable on cube MXThanks for your help !

LMyle.1 by Associate III
  • 5183 Views
  • 11 replies
  • 1 kudos

Resolved! Hi I am concerned about the following microcontroller : STM32H753XIH6TR When using cube Mx to configure the timers on pin PA1_C the options specified in the data sheet are not avaliable. How do I access these functions?

I have downloaded the new H7 package as previously suggested and the issue still remains.Please see attatched image of functions specified in datasheet.Please see image attatched of functions avalailable on cube MXThanks for your help !

LMyle.1 by Associate III
  • 4580 Views
  • 5 replies
  • 0 kudos

Resolved! Problem on SCB_InvalidateDCache_by_Addr

First time try ADC Dual Interleaved on STM32H750VB.The problem is when I try to split the 32bit result from DMABuff into 16bit master and slave, some of the reading is zero and it's random. Can anyone show me anything wrong on my code?If disable DCac...

0693W00000D2FMwQAN.jpg 0693W00000D2FNLQA3.jpg 0693W00000D2FNuQAN.jpg
SEng.1 by Associate II
  • 3112 Views
  • 3 replies
  • 0 kudos

Resolved! clock configuration problem

I use STM32H750XB microcontroller for my project. I am able to configure clock for 480Mhz without using "Resolve Clock Issues" help. But if I use "Resolve Clock Issues" even once, then I get problem like the attached image. There is a calculation err...

0693W00000D27nLQAR.png 0693W00000D27qeQAB.png
OERCA.1 by Associate II
  • 3223 Views
  • 4 replies
  • 0 kudos

STM32F103VG Use Cubemx to generate TIM1 CH1 PWM output, and use firmware version stm32cube FW_ F1 v1.8.1 has normal PWM output. Use firmware version stm32cube FW_ F1 v1.8.1 ~ v1.8.4 cannot output PWM.

 void user_pwm_setvalue(uint16_t value){ TIM_OC_InitTypeDef sConfigOC; sConfigOC.OCMode = TIM_OCMODE_PWM1; sConfigOC.Pulse = value; sConfigOC.OCPolarity = TIM_OCPOLARITY_HIGH; sConfigOC.OCFastMode = TIM_OCFAST_DISABLE; HAL_TIM_PWM_ConfigChannel(&htim...

0693W00000D26CsQAJ.png 0693W00000D26D2QAJ.png
李强.1 by Associate
  • 890 Views
  • 0 replies
  • 0 kudos

O_NONBLOCK is defined twice and does not work with lwIP

The define O_NONBLOCK exists twice. Once in:...\ST\STM32CubeIDE_1.6.0\STM32CubeIDE\plugins\com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.9-2020-q2-update.win32_2.0.0.202105311346\tools\arm-none-eabi\include\sys\_default_fcntl.h:#define _...

PChri.2 by Associate II
  • 4031 Views
  • 7 replies
  • 0 kudos

Resolved! [SOLVED] STM32L0 possible bug with DMA

Hey!I'm trying sending message over UART with DMA with following code and CubeMX configuration (attached pictures)char welcome[] = "hi!\r\n"; HAL_UART_Transmit_DMA(&huart2, (uint8_t*) welcome, strlen(welcome));Nothing else is changed. MCU doesn't s...

VLau by Associate III
  • 3876 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.