STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1756 Views
  • 0 replies
  • 2 kudos

STM32H7 1.9.0 MDMA request not initialized

Specifically I've noticed it with the octospi, but it's also impacted at least software requests.For example, my MDMA config has hmdma_octospi1_fifo_th.Instance = MDMA_Channel1; hmdma_octospi1_fifo_th.Init.TransferTriggerMode = MDMA_BUFFER_TRA...

DShekter by Associate III
  • 2109 Views
  • 3 replies
  • 0 kudos

How to configure QUADSPI in stm32h747bi ?

Hi,I am using stm32h747bi chip in custom board and I want to communicate with GD25Q32C flash memory. I have generated the code for QSPI driver from cubemx. I initialised the GPIO pins as below:/* Peripheral clock enable */  __HAL_RCC_QSPI_CLK_ENABLE(...

SLuit.1 by Associate III
  • 4791 Views
  • 9 replies
  • 0 kudos

Resolved! Clock source for ADC of The STM32H7 CPU

In former CubeMX versions an Clock to ADC of 400MHz was possibleNow I am working on CubeMX V 6.3.0 with STM32Cube FW_H7 V1.9.0.The maximum Clock frequency I can adjust is now 79MHz (selected clock source is the PLL2) What is the meaning of the "79 to...

0693W00000DmOGpQAN.jpg 0693W00000DmOH4QAN.jpg 0693W00000DmODcQAN.jpg 0693W00000DmOMJQA3.jpg

STM32H745 EXTI with STM32CubeMX issue

Hello,I have a question regarding the external interrupt on a GPIO input pint which is triggered each falling edge (EXTI)According to the CubeMX autogenerated code, it looks straight forward. I am using a discovery board with pin PE3 which is config...

PButc.1 by Associate II
  • 3471 Views
  • 5 replies
  • 0 kudos

Interrupt not triggering on NUCLEO-F413ZH

Hi,I have a single PDM mic connected to DFSDM2, channel 0 on the NUCLEO. I have configured the peripheral for 16kHz and I have verified that the clock generated is 1MhZ and the mic sends PDM data when clocked.I have checked the signals going to the u...

0693W00000DmcFbQAJ.png 0693W00000DmcFRQAZ.png 0693W00000DmcFCQAZ.png 0693W00000DmcF7QAJ.png
NKara.3 by Associate II
  • 1306 Views
  • 1 replies
  • 0 kudos

Resolved! STM32CubeMX 6.0.1 with STM32Cube MCU Package for STM32H7 Series version 1.8.0 unchecks the MicroLIB checkbox

Hello,I have an IOC file, which was generated with help of STM32CubeMXMxCube.Version=5.6.1MxDb.Version=DB.5.0.60When I open this project to update the Keil project (which has Keil Compiler version 6 selected), with STM32CubeMX version 6.0.1 (with STM...

Resolved! ffconf.h is missing in stm32CubeMX generated code. STM32G0B0RE

I created new project using CubeMX and selected USB Host and FATFS. but ffconf.h is missing in the project it is giving error.I treid to copy from STM32F769 example project but function is missing. retFATFS = FATFS_LinkDriver(&FATFS_Driver, FATFSPath...

HPATH.1 by Associate II
  • 2427 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.