2021-09-01 5:56 AM
Hi,
When generating code for the STM32H723ZG OCTO SPI2 peripheral it does not generate the __HAL_LINKDMA(ospiHandle, hmdma, hmdma_octospi2_fifo_th); macro for linking the MDMA.
This happens for me when using MDMA channel 2 with the octo spi 2 peripheral configured as quad spi. For now I can fix this issue by adding the __HAL_LINKDMA(ospiHandle, hmdma, hmdma_octospi2_fifo_th) macro manually to the code but it disappears on code generation.
The neccessary macro however is generated on the octo spi 1 peripheral. I have added the CubeMX file with my current configuration.
Also a little code snipped where the macro should be placed.
hmdma_octospi2_fifo_th.Init.SourceBurst = MDMA_SOURCE_BURST_SINGLE;
hmdma_octospi2_fifo_th.Init.DestBurst = MDMA_DEST_BURST_SINGLE;
hmdma_octospi2_fifo_th.Init.SourceBlockAddressOffset = 0;
hmdma_octospi2_fifo_th.Init.DestBlockAddressOffset = 0;
if (HAL_MDMA_Init(&hmdma_octospi2_fifo_th) != HAL_OK) {
Error_Handler();
}
if (HAL_MDMA_ConfigPostRequestMask(&hmdma_octospi2_fifo_th, 0, 0) != HAL_OK) {
Error_Handler();
}
// OFFENDING CODE: The macro below is not added when generating the project.
__HAL_LINKDMA(ospiHandle, hmdma, hmdma_octospi2_fifo_th);
/* OCTOSPI2 interrupt Init */
HAL_NVIC_SetPriority(OCTOSPI2_IRQn, 0, 0);
HAL_NVIC_EnableIRQ(OCTOSPI2_IRQn);
/* USER CODE BEGIN OCTOSPI2_MspInit 1 */
/* USER CODE END OCTOSPI2_MspInit 1 */
2021-09-02 3:56 AM
Hi @JBand.2 ,
Thanks for reporting this issue and sharing the ioc file that helps to reproduce it.
I added relevant topics (Mainly STM32CubeMX) to help our experts (@Khouloud OTHMAN & @Khouloud ZEMMELI ) review it and take the required corrective actions.
-Amel
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2021-09-02 6:46 AM
Hello @JBand.2 ,
I have checked from my side and you're right, I confirm the problem.
Thanks for raising this issue to our attention, it will be fixed.
Thanks for your contribution :)
Khouloud
2021-09-10 2:01 AM
Thank you for the swift response! I am looking forward to the fix.
Thanks!
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.