2021-09-09 9:44 AM
Specifically I've noticed it with the octospi, but it's also impacted at least software requests.
For example, my MDMA config has
hmdma_octospi1_fifo_th.Instance = MDMA_Channel1;
hmdma_octospi1_fifo_th.Init.TransferTriggerMode = MDMA_BUFFER_TRANSFER;
hmdma_octospi1_fifo_th.Init.Priority = MDMA_PRIORITY_VERY_HIGH;
hmdma_octospi1_fifo_th.Init.Endianness = MDMA_LITTLE_ENDIANNESS_PRESERVE;
hmdma_octospi1_fifo_th.Init.SourceInc = MDMA_SRC_INC_BYTE;
hmdma_octospi1_fifo_th.Init.DestinationInc = MDMA_DEST_INC_DISABLE;
hmdma_octospi1_fifo_th.Init.SourceDataSize = MDMA_SRC_DATASIZE_BYTE;
hmdma_octospi1_fifo_th.Init.DestDataSize = MDMA_DEST_DATASIZE_BYTE;
hmdma_octospi1_fifo_th.Init.DataAlignment = MDMA_DATAALIGN_RIGHT;
hmdma_octospi1_fifo_th.Init.BufferTransferLength = 1;
hmdma_octospi1_fifo_th.Init.SourceBurst = MDMA_SOURCE_BURST_SINGLE;
hmdma_octospi1_fifo_th.Init.DestBurst = MDMA_DEST_BURST_SINGLE;
hmdma_octospi1_fifo_th.Init.SourceBlockAddressOffset = 0;
hmdma_octospi1_fifo_th.Init.DestBlockAddressOffset = 0;
if (HAL_MDMA_Init(&hmdma_octospi1_fifo_th) != HAL_OK)
{
Error_Handler();
}
__HAL_LINKDMA(ospiHandle,hmdma,hmdma_octospi1_fifo_th);But what it's missing is the Init.Request. So I had to add
/* USER CODE BEGIN OCTOSPI1_MspInit 0 */
hmdma_octospi1_fifo_th.Init.Request = MDMA_REQUEST_OCTOSPI1_FIFO_TH;
/* USER CODE END OCTOSPI1_MspInit 0 */and that fixed everything. a similar thing was needed for the software request, however there are no USER CODE sections in the init function.
Code was generated with the STM32CubeIDE, version 1.7.0.
2021-09-10 3:38 AM
Hi @Community member ,
Thanks for bringing this issue to our attention.
I let our Expert @Khouloud ZEMMELI review it and take the required corrective actions, if needed.
-Amel
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2021-09-10 3:49 AM
Hello @Community member ,
Could you please share your ioc file to check your case?
Thanks, Khouloud
2021-09-10 4:43 AM
Sure. I've attached an IOC that shows the issue for software and OCTOSPI requests. For me, the initializations look like:
static void MX_MDMA_Init(void)
{
/* MDMA controller clock enable */
__HAL_RCC_MDMA_CLK_ENABLE();
/* Local variables */
/* Configure MDMA channel MDMA_Channel0 */
/* Configure MDMA request hmdma_mdma_channel40_sw_0 on MDMA_Channel0 */
hmdma_mdma_channel40_sw_0.Instance = MDMA_Channel0;
hmdma_mdma_channel40_sw_0.Init.TransferTriggerMode = MDMA_BUFFER_TRANSFER;
hmdma_mdma_channel40_sw_0.Init.Priority = MDMA_PRIORITY_LOW;
hmdma_mdma_channel40_sw_0.Init.Endianness = MDMA_LITTLE_ENDIANNESS_PRESERVE;
hmdma_mdma_channel40_sw_0.Init.SourceInc = MDMA_SRC_INC_BYTE;
hmdma_mdma_channel40_sw_0.Init.DestinationInc = MDMA_DEST_INC_BYTE;
hmdma_mdma_channel40_sw_0.Init.SourceDataSize = MDMA_SRC_DATASIZE_BYTE;
hmdma_mdma_channel40_sw_0.Init.DestDataSize = MDMA_DEST_DATASIZE_BYTE;
hmdma_mdma_channel40_sw_0.Init.DataAlignment = MDMA_DATAALIGN_PACKENABLE;
hmdma_mdma_channel40_sw_0.Init.BufferTransferLength = 1;
hmdma_mdma_channel40_sw_0.Init.SourceBurst = MDMA_SOURCE_BURST_SINGLE;
hmdma_mdma_channel40_sw_0.Init.DestBurst = MDMA_DEST_BURST_SINGLE;
hmdma_mdma_channel40_sw_0.Init.SourceBlockAddressOffset = 0;
hmdma_mdma_channel40_sw_0.Init.DestBlockAddressOffset = 0;
if (HAL_MDMA_Init(&hmdma_mdma_channel40_sw_0) != HAL_OK)
{
Error_Handler();
}
/* MDMA interrupt initialization */
/* MDMA_IRQn interrupt configuration */
HAL_NVIC_SetPriority(MDMA_IRQn, 0, 0);
HAL_NVIC_EnableIRQ(MDMA_IRQn);
}and
/* OCTOSPI1 MDMA Init */
/* OCTOSPI1_FIFO_TH Init */
hmdma_octospi1_fifo_th.Instance = MDMA_Channel1;
hmdma_octospi1_fifo_th.Init.TransferTriggerMode = MDMA_BUFFER_TRANSFER;
hmdma_octospi1_fifo_th.Init.Priority = MDMA_PRIORITY_LOW;
hmdma_octospi1_fifo_th.Init.Endianness = MDMA_LITTLE_ENDIANNESS_PRESERVE;
hmdma_octospi1_fifo_th.Init.SourceInc = MDMA_SRC_INC_BYTE;
hmdma_octospi1_fifo_th.Init.DestinationInc = MDMA_DEST_INC_BYTE;
hmdma_octospi1_fifo_th.Init.SourceDataSize = MDMA_SRC_DATASIZE_BYTE;
hmdma_octospi1_fifo_th.Init.DestDataSize = MDMA_DEST_DATASIZE_BYTE;
hmdma_octospi1_fifo_th.Init.DataAlignment = MDMA_DATAALIGN_PACKENABLE;
hmdma_octospi1_fifo_th.Init.BufferTransferLength = 1;
hmdma_octospi1_fifo_th.Init.SourceBurst = MDMA_SOURCE_BURST_SINGLE;
hmdma_octospi1_fifo_th.Init.DestBurst = MDMA_DEST_BURST_SINGLE;
hmdma_octospi1_fifo_th.Init.SourceBlockAddressOffset = 0;
hmdma_octospi1_fifo_th.Init.DestBlockAddressOffset = 0;
if (HAL_MDMA_Init(&hmdma_octospi1_fifo_th) != HAL_OK)
{
Error_Handler();
}
__HAL_LINKDMA(hospi,hmdma,hmdma_octospi1_fifo_th);
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.