STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1762 Views
  • 0 replies
  • 2 kudos

USB-DFU example bug (STM32H7)

I am showing that USB-DFU example available in latest CubeMX STM32Cube_FW_H7_V1.9.0 package (/Projects/NUCLEO-H7A3ZI-Q/Applications/USB_Device/DFU_Standalone) does not work. The example contains this code:/* Test if user code is programmed starting f...

TDJ by Lead
  • 2307 Views
  • 3 replies
  • 1 kudos

fsfat with freeRTOS

I am using NUCLEO-H743ZI2. I am using STM32CUBEIDE v1.7 with h7 v1.90 to config a application to work with MicroSD card (SDMMC1). After I use stm32cube to config FsFat sdmmc1 , mdma and freertos v1.2. However, the program doesn't work properly. at th...

0693W00000DlRy9QAF.png
yang hong by Associate III
  • 1711 Views
  • 3 replies
  • 0 kudos

Resolved! SYS is in conflict with TIM2_CH1

Hello, MCU: STM32F105VCI am going to use TIM2 to operate in encoder mode with two input channels (combined TI1 & TI2).SYS shows a conflict with TIM2. How can I fix the conflict?Thank You.

NASI by Senior
  • 2873 Views
  • 2 replies
  • 0 kudos

Series of measurements with ADC and DMA on STM32H743

Hi. Can you tell me, why I don't get interrupt from completed measure of ADC. I need to make 200 measeurements using DMA. I have configured settings in CubeMX. You can find them on the screenshot and the part of the code where I run and call it. The ...

DBrau.2 by Associate III
  • 5449 Views
  • 5 replies
  • 0 kudos

Resolved! .

wwgww by Associate II
  • 1617 Views
  • 2 replies
  • 0 kudos

FLASH_SR CFGBSY flag is set after calling HAL_ADC_ConfigChannel() to configure internal temperature sensor on STM32G071

Im initializing my ADC peripheral using the generated MX_ADC1_Init function. At the end of the function, the following snippet is executed:sConfig.Channel = ADC_CHANNEL_TEMPSENSOR;   if (HAL_ADC_ConfigChannel(&hadc1, &sConfig) != HAL_OK) { Error_Hand...

CHoel.2 by Associate
  • 1880 Views
  • 3 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.