STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1757 Views
  • 0 replies
  • 2 kudos

STM32G4 CubeMX SystemClock_Config() generation error ?

I generate a LL code with STM32CubeMx 6.4 for STM32G491.In SystemClock_Config() I get LL_RCC_SetSysClkSource (LL_RCC_SYS_CLKSOURCE_PLL) ; LL_RCC_SetAHBPrescaler (LL_RCC_SYSCLK_DIV_2) ; /* Wait till System clock is ready */ while (LL_RCC_GetSy...

timer with STM32L010c6tx (mikroseconds)

I am using STM32L010c6tx processor I need Microseconds function. How can I do it using a timer? https://www.youtube.com/watch?v=SqC0IhLKJ9o&ab_channel=ControllersTech I did as it shows in the video but the program didn't work. Most likely APB2, presc...

ZKURT.1 by Senior
  • 2233 Views
  • 2 replies
  • 0 kudos

Resolved! STM32F4 HAL I2C Driver Address Problem

I have a problem of the HAL Driver function HAL_I2C_Master_Transmit's parameter 'DevAddress'. It says that the device 7 bits address value in datasheet must be shifted to the left before calling the interface, that is, if I want to transmit to a devi...

Resolved! STM32L4R5ZI gets stuck after initializing I2C

Hello and Thank youI'm starting with I2C on STM32L4R5ZI and I can't get it to work.I'm generating a very simple project for the Nucleo board in CubeIDE.I have only initialize the parameters in CubeIDE, and when I try to run it the red LED ligths up a...

DMart.16 by Associate II
  • 4095 Views
  • 9 replies
  • 0 kudos

Resolved! Two different I2C bus do not work together

Hi!I use two I2C device on two different bus (I2C1 and I2C2) on a STM32G07B1 MCU.The two bus works very well, if I use only one in my code.But if I would like to use all of two, then it will go to HardFault from "__HAL_I2C_GET_FLAG".I use the polling...

0693W00000HohBeQAJ.png 0693W00000HohCIQAZ.png
TKota.3 by Associate
  • 2059 Views
  • 2 replies
  • 0 kudos

Unable to set up SPI between 2 stm32 devices

I am trying to get 2 stm32f411's to communicate via SPI. From my understanding, there should be 1 master device while the others should be its slaves. For my master device, I am using full-duplex master and I have disabled NSS and enabled the NSS pin...

0693W00000Hoa0tQAB.png 0693W00000Hoa1DQAR.png 0693W00000Hoa3nQAB.png
JTurn.2 by Senior
  • 2253 Views
  • 4 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.