STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1756 Views
  • 0 replies
  • 2 kudos

Importing STM32CubeMX to Eclipse

Hello, I am new to STM32 and trying to learn it by migrating from 8 bit PIC. I have started by setting Eclipse environment and created some simple programs. Now I want to use STM32CubeMX but i have problems. I use STM32CubeMX version 5.0.1, and Eclip...

Resolved! How to config the OTFDEC with CubeMX?

I used STM32H730IB but I cannot config the OTFDEC."Warning: This peripheral has no parameters to be configured." when I activated the OTFDEC.

V.H by Senior
  • 1281 Views
  • 1 replies
  • 0 kudos

CubeMX doesn't generate interrupt handle for Time base timer

Hello, I'm using STM32CubeMX 5.5.0 and Discovery board for STM32H747XIHx with FreeRTOS. FreeRTOS uses system tick timer and I use TIM7 as Timebase source, but this issue happen also if I use other timers then TIM7. When my *.ioc project is opened and...

PHlin.1 by Associate III
  • 6207 Views
  • 5 replies
  • 0 kudos

Hello world project clock issue

I have an STM32F415VG custom board with a 25MHz external oscillator.I created an empty project with CubeMX setting the clock to use HSE+PLL to have 72MHz SYSCLK. Nothing else is enabled except the Serial Wire Debug port.I import the project in KEIL, ...

RMais by Associate II
  • 2526 Views
  • 4 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.