2021-12-15 7:37 AM
2021-12-18 4:45 AM
2021-12-15 7:42 AM
Sorry, somehow I managed to drop the question:
During startup, stcube prints a message about log4j. There are known vulnrerabilities about log4j. How does this impact stcube and the host system, stcube runs on?
2021-12-15 9:43 AM
Apparently the version used is so out of date that it's "safe". Not sure I'd trust that answer.
2021-12-15 1:06 PM
I wonder how exactly could an outside attacker achieve an entry to be inserted to CubeIDE/ CubeWhatever's log...
Do these programs have open listening IP ports?
JW
2021-12-15 1:41 PM
It will try to format the log message and if you have certain patterns in the message being logged, it will load an arbitrary file from a web address to do so. So if you can control what is being logged, perhaps if the program logs user input, you're toast.
It is amazing that a program ostensibly designed to log events in a program has gone through so much feature creep that it is even possible for this to happen. I'm not surprised it happened in Java.
I find it all quite interesting.
2021-12-15 7:40 PM
I understand the mechanism of the bug. My question was towards how
> if you can control what is being logged,
can happen in the particular case of Cuben.
JW
2021-12-18 4:45 AM
2021-12-19 5:17 PM
> It is amazing that a program ostensibly designed to log events in a program has gone through so much feature creep
That is also the past and future of the CubeMX. It started as a Microcontroller eXplorer and helped managing pins and clocks. Then the "initialization code generator" was added. Officially it's still called like that! But in reality it has gone down the full - "I'm clicking a project together completely in CubeMX. Something doesn't work. I no learn C. Help!!! Thank you, ser!" - mode. And even sane users want more and more customization. Initialization order, priorities, enable/disable by default etc. Eventually it will mimic all of the HAL in a million configurations, it will require the same amount of knowledge and be more complex to configure than writing a code, and the project will collapse under it's own weight.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.