STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1756 Views
  • 0 replies
  • 2 kudos

Resolved! STM32H7B0VB Max Clock

Hi, I'm trying to configure my stm32h7b0vb for max clock (280Mhz), but max freq on DIVN1 is 420Mhz, and DIVP1 is 2 (min val). Therefore I only reach 210Mhz

0693W00000Kbff4QAB.png
MMira.4 by Associate II
  • 7418 Views
  • 3 replies
  • 0 kudos

Some problems with STM32Cube after updating software

Hello,I haven't used STM32Cube for a long time because I was busy with other things.For software and hardware development I use STM32Cube under Linux and the board NUCLEO-H743ZI2 as hardware platform.Since I wanted to create an project from scratch, ...

Resolved! FDCAN config issues with STM32H747I-EVAL board

Hello dear community,This is my first post here and I am coming to you for help.In the context of a project with a STM32H747I-EVAL board (this board was lent to me and I notice that it doesn't seem to be sold anymore), I need to send/receive CAN mess...

Pampah by Associate
  • 2034 Views
  • 1 replies
  • 0 kudos

Resolved! STM32F372/STM32F373 as a USB host

When I was going through the setup process of USB in STMcubeMX, I suspected that it could not be used as USB host.I would like to know if STM32F372/STM32F373 can be used as USB host. Can STM32F372/373 be used as USB host?

FLast.5 by Associate II
  • 2389 Views
  • 3 replies
  • 0 kudos

STM32CubeIDE - want create new C++ executable (File > New > STM32 Project), takes me to STM32CubeMX, after configuration, next step?

Requirement: I need to create a basic C++ project (into which I'll insert files from an embedded C++ project built for another platform, then begin port testing.) The specifics are using a STM32F051R8 with "LL" low level support, but I don't think my...

wb0gaz by Senior
  • 3085 Views
  • 3 replies
  • 0 kudos

After programming going to execute not happening. I normally keep the controller in boot mode and load the code either through serial port or USB depending on the controller. In this case it is 103C8 controller. I use STM CUBE Programmer.

I tick the "Run after programming" option. Normally this works fine. User code gets going after programming. I create projects using Cube MX. With latest Cube MX (Version 6.4.0) code, after programming control is not going to user code. I have to now...

How to receive SPI in Half-duplex-Mode?

Hallo,i dont unterstand how i can receive data in Spi Half-Duplex-Mode.My used Controller is STM32F446RET.STM32CubeMX is configured as followThats my Code: HAL_GPIO_WritePin(CS_GPIOxLib, CS_GPIO_PinLib, GPIO_PIN_RESET);           status = HAL_SPI_T...

0690X000006DN9cQAG.png 0690X000006DN9mQAG.png 0690X000006DNA1QAO.png 0690X000006DNAfQAO.png
mfrank9 by Associate III
  • 6899 Views
  • 5 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.