STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1756 Views
  • 0 replies
  • 2 kudos

Resolved! UART DMA not work with STM32F767ZI and STM32F745VE

Hi Team​UART DMA not works with STM32F767ZI and STM32F745VE.It does not transmit or receive data.​Testing same code with STM32F405 and STM32G474, UART DMA works fine.​Does anyone know why UART DMA doesn't work on STM32F?Is there anything to be care o...

0693W00000KaLImQAN.png
Kenji1 by Senior
  • 7015 Views
  • 10 replies
  • 1 kudos

Resolved! How to: CubeMX + FreeRTOS + CrossStudio

I am trying to add FreeRTOS support in an STM32CubeMX project, and import into Rowley CrossStudio.In CubeMX, I have tried all toolchains, and then import them into CrossStudio.But none of them works, and I get a ton of compiler errors.When generating...

KKjel.1 by Senior
  • 4513 Views
  • 11 replies
  • 0 kudos

Resolved! Bug Report on Code Generation for STM32H745 using STM32CubeMX V6.4.0

The PB7 pin is set as GPIO_EXTI7 and TIM17 is enabled for PWM output. In the generated code, the IRQ routine is generated wrongly as follow:void EXTI9_5_IRQHandler(void) { /* USER CODE BEGIN EXTI9_5_IRQn 0 */   /* USER CODE END EXTI9_5_IRQn 0 */ ...

PX by Associate II
  • 1996 Views
  • 2 replies
  • 0 kudos

Resolved! Dear all, I use Cube Mx to generate code for good start and I made a project with STM32F745VETx. PD8 is set as EXTI8 and interrupt is activated. PE8 is defined as normal input.

When I generate the code, Cube MX generates interrupt handler for EXTI9_5 and it is like that: /* USER CODE END EXTI9_5_IRQn 0 */ HAL_GPIO_EXTI_IRQHandler(DIN2_Pin); /* USER CODE BEGIN EXTI9_5_IRQn 1 */DIN2_Pin actually corresponds to PE8 and it is n...

TA1 by Senior
  • 2932 Views
  • 6 replies
  • 0 kudos

Resolved! STM32CubeMx Code generation inconvenient

STM32CubeMx will generate the code as below.HAL_GPIO_EXTI_IRQHandler (GPIO_OUTPUT_PA0_Pin);But I want it to be generated as follows:HAL_GPIO_EXTI_IRQHandler (PB0_EXTI0_Pin);orHAL_GPIO_EXTI_IRQHandler (GPIO_PIN_0);The user label of the pin assigned to...

tsuna by Associate II
  • 1407 Views
  • 2 replies
  • 0 kudos

STM32CubeMX 6.5.0 released

What is new in STM32CubeMX V6.5.0? • Added the support for new part numbers in the STM32U5 Series: STM32U599NJHxQ, STM32U599BJYxQ, STM32U595ZJTxQ, STM32U5A9NJHxQ, STM32U5A9BJYxQ, STM32U5A5ZJTxQ and STM32U599NIHxQ. • Added the support for new part num...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.