STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1759 Views
  • 0 replies
  • 2 kudos

STM32L152 UART5 Pull Up forced by Mx?

I am trying to configure the UART5 on PD2 and PC12 for my STM32L152RE as open drain but the Mx GUI only offers pull ups. I searched manual and Errata but nothing indicates a special pin here. is this a bug in the Mx config or a real thing does anybo...

ASche.5 by Associate III
  • 1519 Views
  • 2 replies
  • 0 kudos

Best/easiest way to share data between cores in STM32H745

I am working with a dual core H7 for the first time and and very confused about how to share data between the two cores. I would like to use the M4 as a slave/background processor for the M7 where the M7 can alert the M4 when there is new data to pro...

RMcCa by Senior II
  • 25598 Views
  • 16 replies
  • 4 kudos

Obtain 48kHz sample rate from SAI on STM32L5

Is it possible to obtain a (theoretical) 48kHz sample rate with 0% error on the STML5's SAI peripheral? So far the clock configuration tool in STM32CubeIDE has been unable to do so.Research led me here, but this is not applicable to a slower clocking...

0693W00000Kd9V6QAJ.png 0693W00000Kd9W9QAJ.png
JTedot by Associate II
  • 1557 Views
  • 1 replies
  • 0 kudos

Resolved! Can you have too many peripheral init functions?

Here is a weird one for ya.I am programming on the STM32L4R9I-EVAL dev board, but my project is configuredfor the STM32L4S9AII6. I am clocked at 120MHz.My program has started failing for what seems to be because I have too manyMX_<peripheral>_init() ...

0693W00000KcBcqQAF.png
MFolk.1 by Senior
  • 5809 Views
  • 10 replies
  • 0 kudos

Unknown error during running code on STM32F105R8

Hi all, I have made a source code that runs fine, But after 6 months I again tried to run the same code. Now the running stuck at some point,The code stuck at this point is shown belowIs this error occur due to any hardware failure like oscillator /c...

0693W00000KcfPYQAZ.png

Use SPI to to manage ADS1118

Hello everybody!Sorry for the question but i am in need of help.I use STM32CubeIDE 1.5.1 with stm32 discovery f407g to manage an exyernal adc ADS1118.ADC works well with Arduino, but unfortunately I can't get it to work with discovery.... /* USER COD...

FItal by Associate II
  • 1879 Views
  • 2 replies
  • 0 kudos

Resolved! stm32l4r9xx.h gives a warning about passing argument 2 of HAL_GPIO_WritePin makes Integer from Point without a cast

Hello STM32-Community,I've got a somewhat mundane problem today. Suddenly a piece of .h file decides to give a warning. I'm using STM32CubeMX and have also rebuilt the project multiple times and I still get this warning: Anyone knows how to fix this ...

0693W00000KcYRWQA3.png
crackl1ng by Associate III
  • 3922 Views
  • 7 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.