STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1757 Views
  • 0 replies
  • 2 kudos

Resolved! H743+FreeRtos+LWIP errno bug?

Hi everyone. After some updates of CubeIde I have returned to an old project and can not compile it. IDE shows me the error of multiple definitions of errno variable. I tried to start a clean project. When I enable FreeRtos and LWIP it shows me the s...

CubMX 6.5.0 ADC issue with STM32G0

Hallo,after Upgrading to CubeMX 6.5.0 there are problems using ADC1 with STM32G070RBT6. When the 'Number of Conversion' > 1 it is not possible to set 'Discontinuous Conversion Mode' to Disabled (only Enabled), with CubeMX 6.4.0 it works. Is this a bu...

I have a question about the external flash loader.

helloI am developing an external flash loader with stm32g070.There is something I don't understand about this.1. Should I use only the internal clock for external flash loader, not the external crystal?2. Can't I use the interrupt?Please reply to the...

lhwa .1 by Associate II
  • 1309 Views
  • 1 replies
  • 0 kudos

Cubeide ADC DMA code generation sequence problem

I am using CUBEIDE 1.9.0.Stm32f103ret6 is used.The ADC generated a code to use DMA.However, it did not work properly.The cause should have been __HAL_RCC_DMA1_CLK_ENABLE() before this ADC was initialized.I tried to modify the DMA initialization faste...

MagicFly by Associate
  • 1893 Views
  • 2 replies
  • 1 kudos

Resolved! Trouble with custom bootloader and CubeMX generated code

Hi, I've got an project in cubeide that starts in one project and then jump's to another at 0x0800C000. It's been working in the past and I've somehow broken it trying to do updates. Here is the main code in the bootloader. It's very simple. BOOTLOAD...

xrstokes by Associate III
  • 1955 Views
  • 2 replies
  • 0 kudos

Using basic timer to trigger ADC conversion

Hi,Using an STM32G4, I want to start an ADC conversion periodically using an event from a timer.To do so I choose the TIMER6 (basic timer) and ADC2 peripherals.Sadly, it didn't work.The reference manual, seems to imply that you can't use a basic time...

0693W00000KdTREQA3.png 0693W00000KdTSCQA3.png
GBert.2 by Senior
  • 1645 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.