STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1756 Views
  • 0 replies
  • 2 kudos

Resolved! Bug in STM32CubeMX for H753 ADC and work-around.

I have problems porting a H743Zi2 code to a H753. When using the .ioc file editor with the ADC the option to set the ADC clock prescalar is not present for the H753. It is there for the H743. The coeersponding line in the main.c code is not present e...

HWhit.1 by Associate III
  • 1801 Views
  • 2 replies
  • 0 kudos

Resolved! [Bug for MPU LL code generation for H755]

I am using CubeIDE Version: 1.6.0 Build: 9614_20210223_1703 (UTC) to initialise the MPU as it is done for the TCP_Echoserver, however the LL resulting code does not set the LL_MPU_TEX_LEVEL1 bit for the second regionGenerated code:/* MPU Configuratio...

0693W000008w0bjQAA.png
Marco.D by Associate II
  • 2594 Views
  • 3 replies
  • 0 kudos

Resolved! STM32CubeL4 v1.17.1 OSPI Delay Block Bypass Problem

The latest versions of the STM32CubeL4 drivers (1.17.1) and CubeMX (6.5.0) introduce two bugs related to the OSPI and Delay Block Bypass.In stm32l4xx_hal_ospi.c line 383, the MODIFY_REG macro no long clears the DLYBYP bit. It also fails to set it acc...

ebray by Associate II
  • 2532 Views
  • 3 replies
  • 0 kudos

Resolved! [STM32L151] STM32CUBEIDE 1.9.0, FW_L1 V1.10.3 SPI1 and SPI2 are missing options to set Clock Polarity (CPOL) and Clock Phase (CPHA)

 I was able to resolve by adding to SPI2_Init  /* USER CODE BEGIN SPI2_Init 1 */ hspi2.Init.CLKPolarity = SPI_POLARITY_HIGH; hspi2.Init.CLKPhase = SPI_PHASE_2EDGE;But STM32CubeIDE 1.8.0 with same version FW_L1 V1.10.3 does have the options as below ...

0693W00000NpjEqQAJ.png 0693W00000NpjhnQAB.png

Custom board with STM32G431 behaves weird

I've done a simple board with a STM32G431, the idea is to be a remote control that drives an infrared led. It has 8 buttons and the MCU should sleep until a button is pressed, then transmit the code and sleep again.Right now I'm just trying to make t...

0693W00000NsneZQAR.png
BRapo.1 by Associate II
  • 1573 Views
  • 1 replies
  • 0 kudos

What fastest way to change the size of the DMA addressed by a peripheral. In particular the DAC? Stopping and starting the DAC using HAL_DAC_Stop_DMA and HAL_DAC_Start_DMA with a new Data Length takes up a lot of cycles if I use the CubeMX functions. I

I tried DMA_SetConfig after __HAL_DMA_DISABLE and clearly it is not enough.Incidentally my intention is not change the size of the DMA allocated area - rather the size of this region accessed by a peripheral

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.