STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1757 Views
  • 0 replies
  • 2 kudos

Documentation for ST scheduler

HelloFor a project that I am working on I need a simple scheduler, a full RTOS is more complex than I need. My first idea was to build one myself but I noticed that when using STM32Cube to generate code to for example run bluetooth a scheduler is inc...

OTern.1 by Associate
  • 2068 Views
  • 1 replies
  • 0 kudos

I can't generate code from stm32cubemx

The first time I generate code, it works.But by the second time I clicked the GENERATE CODE, the progress bar is not moving anymore after 'generating user source code'.I have tried to remove the file '.mxproject' , but it didn't work. The Application...

0693W00000NsliKQAR.png
Lkid by Associate
  • 1511 Views
  • 2 replies
  • 0 kudos

how to stop output compare channel at only 8 pulses?

I have used output compare to send data at two pins simultaneously. the data is variable. however, I need only 8 clk pulses and on each rising and falling pulse edge data transfer to the output pin.I am unable to stop pulses and data at only 8 edges ...

0693W00000NsrrhQAB.png 0693W00000NsrpbQAB.png 0693W00000NsrpgQAB.png 0693W00000NsrwXQAR.png
SAMIN.1 by Associate III
  • 867 Views
  • 0 replies
  • 0 kudos

Resolved! Is the STM32H747 code directly portable to the STM32H757?

I'm using the STM32H757i Eval board. In STMCube repository for H7 v1.10.0, there is not a project folder for the STM32H757i eval board. I'd like to use the BSP LED/Touch drivers from the STM32H747i-EVAL project found in the cubeMX repository and pote...

jmorganj by Associate III
  • 1268 Views
  • 1 replies
  • 0 kudos

Resolved! The instructions in UM1718 Rev 37 Chapter 15, page 292 compatible processors is running for 4 hours and is only 50% done.

I have STM32CubeIDE 1.9.0 and I am editing the .ioc. In the Pinout & Configuration Tab I right click and select List Pinout Compatible MCUsIt starts runningand running and running. Last night I let it run all night and it said it was 8% and there was...

KiptonM by Lead
  • 2220 Views
  • 2 replies
  • 0 kudos

Resolved! Bugs in LL driver for STM32H743

MCU:stm32h743vih6 rev.vSTM32CubeMX Ver:6.4.0Configuration: HSE 16MHz, 480MHz cpu core frequency, system clock mux=pllclk(480MHz), HPRE Prescaler=4. Project manager -> Advance Settings -> Driver Selector -> GPIO/RCC/CORTEX_M7 all set to LL.Bug: mcu wi...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.