STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1756 Views
  • 0 replies
  • 2 kudos

Enable 48MHz HSE on STM32F446RE Nucelo

On the board page nucleo-f446re it mentions a specific feature of board is a 48MHz HSE. However in STM32CubeIDE I only have the option to set the HSE up to 26MHz. How do I go about enabling the 48MHz HSE or could you point me in the direction of any ...

0693W00000QLuakQAD.png

While programming with the JLink Ultra, it reports 2 device on the JTAG bus, I am using one STM32L471RGT6. Is this correct? Programming and running code mainly works but not always.

Connecting to target...J-Link found 2 JTAG devices, Total IRLen = 9JTAG ID: 0x4BA00477 (Cortex-M4)Connected to targetWaiting for GDB connection...Connected to 127.0.0.1Reading all registersRead 4 bytes @ address 0x080014B0 (Data = 0xF00369DB)Reading ...

rwils.1 by Associate III
  • 2225 Views
  • 4 replies
  • 0 kudos

STM32cubeIDE Board Selector creates incorrect (?) default RCC initialization settings for STM32H735G-DK Discovery Kit.

@Piranha​ pointed me to a fault in the configuration of the RCC in an example related to LW-IP.I have the impression that this fault is also created when STM32cubeIDE creates the default settings for the STM32H735G -DK Discovery kit.The manual RM0468...

0693W00000QM6E2QAL.png 0693W00000QM6AFQA1.png 0693W00000QM6AZQA1.png 0693W00000QM6AtQAL.png
Johi by Senior III
  • 853 Views
  • 0 replies
  • 1 kudos

Resolved! Dma not working when triggered from timer trigger from external source start a DMA transfer on UART or SPI peripheral on STM32F411?

I am using STM32F411 and SDK v1.27.1I am trying to trigger an DMA xfer with an external signal source using the TIMER1 External Trigger, without the need to execute any interrupts in the CPU to utilize the CPU time, as I have two signals one every 2m...

0693W00000QLM9zQAH.png 0693W00000QLMA4QAP.png 0693W00000QLMAdQAP.png 0693W00000QLMA9QAP.png

Resolved! Nucleo-F072RB Multi-channel ADC Problem

Hello. I want to read multi-channel analog data (four channels) with my Nucleo-F072RB. I previously worked with Nucleo F411RE and I did not have any problems. But with F072RB, I'm so confused. When I open my board on CubeMX, I can select multi ADC1 c...

MÇeli.2 by Associate II
  • 3742 Views
  • 4 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.