2022-03-14 4:11 AM
Since CubeMX changed to 6.5.0 and Firmware Package to V1.10.0 (included full-reworked ETH driver) Ethernet on existing project became not work after code regeneration.
Detailed investigation shows that:
Software example that supplied with Firmware Package (LwIP_HTTP_Server_Netconn_RTOS) works fine and free of issues, described above.
But ethernetif.c, generated by CubeMX, needs to be corrected manually.
Also, it seems have to change Cortex_M7 memory regions settings exactly as in software example.
2022-03-18 2:55 AM
I was alone with a code that didn't work after the update. Thanks for reporting the bug. It was very helpful.
2022-03-28 3:35 AM
Hi @Community member,
Thanks for sharing your finds.
It is worth to bring it to the attention of our STM32CubeMX experts @Sara BEN HADJ YAHYA and @Khouloud OTHMAN to more investigate & share with us taken actions.
-Amel
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2022-06-21 2:16 AM
@Amel NASRI @Sara BEN HADJ YAHYA @Khouloud OTHMAN
Any update on this?
Same issue is also reported here: https://community.st.com/s/question/0D53W00001TgW6xSAF/project-generation-for-stm32h7-with-freertos-lwip
2022-06-21 6:22 PM
For those who pressed the Migrate button, you can revert to the working version by editing the IOC file with a text editor and changing the parameters as below:
ProjectManager.FirmwarePackage=STM32Cube FW_H7 V1.9.0
MxDb.Version=DB.6.0.21
2022-07-11 12:30 PM
I also had the second bug mentionned in this post after migrating to latest firmware package!
Please fix this! it looks like an easy fix !
"In the function ethernet_link_thread() at section under if(linkchanged){} used HAL_ETH_Start(&EthHandle); instead of HAL_ETH_Start_IT(&EthHandle);. That stops ETH after reconnect a cable.
2022-07-11 1:40 PM
@Community member Do you have the latest? CubeMX 6.6.1 or IDE 1.10.1?
2022-07-11 2:44 PM
@Pavel A. Yes, I got the latest IDE (1.10.1) just today and i'm using STMfirmware package 1.17 for stm32F7
2022-07-20 8:18 AM
With CubeF7 v1.17 the F7 series also have been struck by this:
Anyway, follow this topic:
2022-07-22 12:38 PM
Guys, my recommendation, stop using the ETH+LWIP implementation from ST. There are problems since years and they do not manage to get a real stable setup, even with the new driver.
In my application I needed a high reliable and high speed data communication (TCP) in an STM32H743. I've fought for months against LWIP but I had to give up. The speed was good but after 10 hours the STM stopped sending packets, it was just not reliable and unsuited for a high availability application.
I have switched to FreeRTOS+TCP and IT IS A BREEZE. It runs for days, weeks, w/o an issue. The integration is not that difficult either and the guys in the community forums are very supportive and have good knowledge:
https://www.freertos.org/FreeRTOS-Plus/FreeRTOS_Plus_TCP/index.html
Finally an ETH Stack that WORKS!
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.