2022-07-25 9:17 AM
Connecting to target...
J-Link found 2 JTAG devices, Total IRLen = 9
JTAG ID: 0x4BA00477 (Cortex-M4)
Connected to target
Waiting for GDB connection...Connected to 127.0.0.1
Reading all registers
Read 4 bytes @ address 0x080014B0 (Data = 0xF00369DB)
Reading 64 bytes @ address 0x20017F80
Received monitor command: WriteDP 0x2 0xF0
O.K.
Received monitor command: ReadAP 0x2
O.K.:0xE00FF003
Read 4 bytes @ address 0x20017FDC (Data = 0x41000000)
Reading 64 bytes @ address 0x20017FC0
Read 4 bytes @ address 0x080005F8 (Data = 0x2B00681B)
Reading 32 bytes @ address 0xE00FFFD0
Read 1 bytes @ address 0x200003BC (Data = 0x0D)
Connected to 127.0.0.1
Reading all registers
Read 4 bytes @ address 0x080014B0 (Data = 0xF00369DB)
Reading 64 bytes @ address 0x20017F80
Received monitor command: reset
Resetting target
Downloading 392 bytes @ address 0x08000000 - Verified OK
Downloading 16016 bytes @ address 0x08000190 - Verified OK
Downloading 15984 bytes @ address 0x08004020 - Verified OK
Downloading 9068 bytes @ address 0x08007E90 - Verified OK
Downloading 512 bytes @ address 0x0800A1FC - Verified OK
Downloading 8 bytes @ address 0x0800A3FC - Verified OK
Downloading 4 bytes @ address 0x0800A404 - Verified OK
Downloading 4 bytes @ address 0x0800A408 - Verified OK
Downloading 212 bytes @ address 0x0800A40C - Verified OK
Writing register (PC = 0x 8001764)
Read 4 bytes @ address 0xE000ED14 (Data = 0x00000200)
Read 4 bytes @ address 0x08001764 (Data = 0xD034F8DF)
Read 2 bytes @ address 0x08001764 (Data = 0xF8DF)
Read 2 bytes @ address 0x08001766 (Data = 0xD034)
Downloading 4 bytes @ address 0xE000ED14 - Verified OK
Reading all registers
Read 4 bytes @ address 0x08001764 (Data = 0xD034F8DF)
Read 2 bytes @ address 0x08001764 (Data = 0xF8DF)
Read 2 bytes @ address 0x08001766 (Data = 0xD034)
Read 4 bytes @ address 0xE000EDFC (Data = 0x01000000)
Downloading 4 bytes @ address 0xE000EDFC - Verified OK
Reading all registers
Read 4 bytes @ address 0x08001764 (Data = 0xD034F8DF)
Read 2 bytes @ address 0x08001764 (Data = 0xF8DF)
Read 2 bytes @ address 0x08001766 (Data = 0xD034)
Reading 64 bytes @ address 0x08000580
Read 2 bytes @ address 0x080005AA (Data = 0xF001)
Read 1 bytes @ address 0x200003BC (Data = 0x0D)
Setting breakpoint @ address 0x080005AA, Size = 2, BPHandle = 0x0001
Starting target CPU...
...Breakpoint reached @ address 0x080005AA
Reading all registers
Removing breakpoint @ address 0x080005AA, Size = 2
Read 4 bytes @ address 0x080005AA (Data = 0xF904F001)
Reading 64 bytes @ address 0x20017FC0
Read 1 bytes @ address 0x200003BC (Data = 0x00)
Starting target CPU...
2022-07-25 12:11 PM
There are two JTAG devices, one for controlling the Pins via boundary scan and the other giving access to the Cortex core. Have a look at the reference manual, e.g. 41.6 in RM0392
2022-07-25 2:16 PM
Well that's a surprise! Thanks very much for taking the time to answer,
2022-07-25 9:39 PM
Hi and also, do you really need to use jtag. Because if HW allow you to connect with SWD, you can get full power of debug session...
Generally JTAG is more usefull for test production of HW.
2022-07-26 6:15 AM
The number of things I don't know are increasing daily! I'm migrating from MSP430 to the cortex and it's a bit of a steep curve. I'll try the SWD link if it works better. What are the debugging advantages? I'm already able to use breakpoints with Jtag but maybe there are additional features I am missing out on.
Thanks for the reply BTW
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.