STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1756 Views
  • 0 replies
  • 2 kudos

Resolved! about STM32CubeMx

This morning, I installed cubemx and created a project for STM32F767IGT6 using J-link v2 to download the hex file to the board, but it didn't work. The project have included the LTDC, but I cannot get any signal(DCLK/VSYNC/HSYNC) from the test pads o...

JChen.37 by Associate II
  • 3444 Views
  • 5 replies
  • 0 kudos

Resolved! STM32H735RGV6 maximum external crystal frequency

Hello dear,I will use "STM32H735RGV6" with an external crystal. In the datasheet, it is stated that "External oscillators: 4-50 MHz HSE". However, in CubeIde I cannot assign 50MHz since it is limited to 48MHz. Could you help with this issue?

Resolved! Confused about input capture channels

Id like to write a program to read 2 main frequencies, first one from velocity sensor and second from ignition coil. Both of them to build a car gauge dashboard, (there'll be a few more analog signals to read tough).Given that i come from atmega 328 ...

JLp.1 by Associate II
  • 3569 Views
  • 6 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.