2022-09-26 8:38 PM
Id like to write a program to read 2 main frequencies, first one from velocity sensor and second from ignition coil. Both of them to build a car gauge dashboard, (there'll be a few more analog signals to read tough).
Given that i come from atmega 328 that has only one input capture module, id like to know if the stm bluepill has the capacity to read both frequencies in the same chip...
I'll need to read 2 frequencies, read analog signals, writing steps bits to update gauges and display data in tft 2.4'' module, so im lookinf for advice about selecting the right chip
Regards
Julian
Solved! Go to Solution.
2022-09-29 11:39 PM
Hello @JLp.1 (Community Member)
About the right chip, the best way is to use STM32CubeMX MPU/MCU Selector. This will help you find the right device for your needs.
Take a look at STM32 Ecosystem there is a whole series of dev board (Nucleo, DK...)
Here the link of good starting point:
STM32 MCU Developer Zone - STMicroelectronics
Thank you to Please my answer as answered.
Best regards,
Romain,
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2022-09-27 11:30 PM
Hello @JLp.1 (Community Member)
STM32F103C8 Datasheet (DS5319 Rev 18) embeds 4 16bit TIMER.
They all have at least 4 GPIOs capable of capturing input and thus making period/frequency/duty cycle measurements.
You can also refer to AN4013 STM32 cross-series timer overview chapter 2.3 for an input capture mode.
From a firmware point of view, you should look at the STM32CubeF1 library example
Let me know if it will help and clarifies your request ?
Best regards,
Romain
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2022-09-28 12:55 AM
One additional comment: if you really want to use this board called Blue Pill, you should know that the STM32s installed there are usually counterfeits, i.e. not originals from STMicroelectronics, even if they look like it. In many cases, they behave completely differently from the originals. So don't be surprised if something doesn't work as expected.
Regards
/Peter
2022-09-29 7:44 PM
It certainly clarifies. Thanks.
About the right chip to do the job I mentioned, what do you think?
Remember, need to read and proccess two frequencies (khz not more than that), update about 10 digital pins, diplay data through spi and drive some neopixels strips....
Would you think 32F103 is enough?
kind regards
julian
2022-09-29 7:46 PM
I had heard such a complain about those modules...
Is there a way to test the module to know wheter the st on board is original or clone ? I've bought a few already....
regards
julian
2022-09-29 11:39 PM
Hello @JLp.1 (Community Member)
About the right chip, the best way is to use STM32CubeMX MPU/MCU Selector. This will help you find the right device for your needs.
Take a look at STM32 Ecosystem there is a whole series of dev board (Nucleo, DK...)
Here the link of good starting point:
STM32 MCU Developer Zone - STMicroelectronics
Thank you to Please my answer as answered.
Best regards,
Romain,
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2022-09-29 11:42 PM
Well, STMicroelectronics manufactures the STM32 originals and also guarantees their functioning, but of course cannot make any statements about any replicas or clones. The Blue Pill board in particular has attracted attention in recent years for using STM32F103 fakes. This will probably not be noticed if you only flash an LED with it.
However, I have seen websites somewhere in the maker scene that deal with distinguishing fakes from originals, e.g. on Greaseweazle's Github account.
In my opinion, however, there is no point in spending much time on this, as the probability of finding a Blue Pill with an original STM32 is close to zero.
Regards
/Peter
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.