STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1756 Views
  • 0 replies
  • 2 kudos

Resolved! Problem reading the RTC calendar after re writing it.

Hello. I'm trying to make a code to show some menús (configuration and user menús) in a LCD screen, but something goes wrong when I try to write the year, and read it later, from the RTC calendar registers.My main code begins with the cube MX functio...

Resolved! STM32G070CB: STM32CubeMX Ver 6.8.0

Hi In my MX setup, using STM32G070CB, I tried to allocate PB11 as ADC_IN15 and PB12 as ADC_IN16. Funny enough, the PB11 & PB12 pins are changed in yellow colours, While PB10 as ADC_IN11 bears no problem with the normal green colour allocated.Hoverin...

STM32H750XBH6 Data Flash Memory for Application Data.

Does the STM32H750XBH6 have data flash memory that I can use to store 200 bytes of application data? For example to store the IP address etc.. The datasheet says something about "2 Kbytes (64 flash words) of user option bytes for user configuration"....

Roger.ch by Associate III
  • 1820 Views
  • 2 replies
  • 0 kudos

Resolved! STM32H745 stuck waiting for M4

I just got started with a dual core STM32H745. I put together a quick project with CubeMX to test some FDCAN interfaces. I built the program and ran it.I'm using Keil ARM MDK. After building, and connecting it appears to connect to the CM7 (which ...

Resolved! No SDIO in CubeMX

Good afternoon.I am using BluePill STM32F103C8T6 board.I wanted to connect an SD card to it and use it as Mass Storage​All examples use the SDIO interface for connection.But I don't have this item in CubeMX. How can I mount an SD card​

_legacyfs_online_stmicro_images_0693W00000biIGNQA2.png
DMukh.2 by Associate II
  • 5860 Views
  • 6 replies
  • 0 kudos

STM32CubeMX 6.8.0 released

We are pleased to announce you that the official release of STM32CubeMX v6.8.0 is available for download hereWhat is new in STM32CubeMX V6.8.0?• Added the support for the STM32H5 series microcontrollers• Added the support for new microcontrollers in ...

How to make the right connection for using DDR Test Suite?

The board is installed with the system( stm32mp1-openstlinux-5.15-yocto-kirkstone-mp1-v22.06.15) by following the Getting started .All drivers are installed.However, in the DDR test suite, I cannot connect to the device.How to make the right connecti...

0693W00000QMwtvQAD.jpg 0693W00000QMx0DQAT.jpg 0693W00000QMx03QAD.jpg

STM32H7, MX make HAL without ISR?

On an STM32H7, is it possible to configure CubeMX to make a HAL that does not use an ISR? It makes one for Tick to increment the tick counter.

DRook.2 by Associate II
  • 1171 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.