2023-04-18 12:51 PM
Hello. I'm trying to make a code to show some menús (configuration and user menús) in a LCD screen, but something goes wrong when I try to write the year, and read it later, from the RTC calendar registers.
My main code begins with the cube MX function that sets a initial value to all the RTC calendar fields:
sTime.Hours = 0x09;
sTime.Minutes = 0x30;
sTime.Seconds = 0x00;
sTime.DayLightSaving = RTC_DAYLIGHTSAVING_NONE;
sTime.StoreOperation = RTC_STOREOPERATION_RESET;
if (HAL_RTC_SetTime(&hrtc, &sTime, RTC_FORMAT_BCD) != HAL_OK)
{
Error_Handler();
}
sDate.WeekDay = RTC_WEEKDAY_FRIDAY;
sDate.Month = RTC_MONTH_MARCH;
sDate.Date = 0x31;
sDate.Year = 0x23;
if (HAL_RTC_SetDate(&hrtc, &sDate, RTC_FORMAT_BCD) != HAL_OK)
{
Error_Handler();
}Later, I can configure the time and date, using some enums to do it more human, in the exit section of a configuration menú:
if (new_exit == 1)
{
date_final.Date = day_enum;
date_final.Month = month_enum;
date_final.Year = year_enum;
HAL_RTC_SetDate(&hrtc, &date_final, RTC_FORMAT_BIN);
time_final.Hours = hour_enum;
time_final.Minutes = minute_enum;
time_final.Seconds = second_enum;
HAL_RTC_SetTime(&hrtc, &time_final, RTC_FORMAT_BIN);
new_entry = 1;
new_exit = 0;
}For example, I can set the date = 31, month = 03, year = 23, and so on...
And finally, in an user menú, I wanted to show the time and date, reading the calendar again, using the following code:
void fm_calendar_get()
{
__HAL_RTC_WRITEPROTECTION_DISABLE(&hrtc);
HAL_RTC_WaitForSynchro(&hrtc);
__HAL_RTC_WRITEPROTECTION_ENABLE(&hrtc);
HAL_RTC_GetTime(&hrtc, &sTime, RTC_FORMAT_BIN);
HAL_RTC_GetDate(&hrtc, &sDate, RTC_FORMAT_BIN);
}But when I read the date, the year is always wrong, it's different than the year I selected before.
I think it is because of the BCD representation of the RTC, but I really don't know how to solve it.
I can give the whole code if it's needed, but it is really a mess, and you will need to configure some buttons to recreate the error...
Solved! Go to Solution.
2023-04-18 2:28 PM
Initialize the whole struct used to write time and date.
Cube is open source. Single step it in debugger to see, what is happening.
JW
2023-04-18 2:28 PM
Initialize the whole struct used to write time and date.
Cube is open source. Single step it in debugger to see, what is happening.
JW
2023-04-19 6:12 AM
You are totally right, it's the second time someone show me that web page, and I think it's fantastic.
Thanks a lot.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.