STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1756 Views
  • 0 replies
  • 2 kudos

Resolved! How to install STM32CubeMX on Ubuntu?

I ran "SetupSTM32CubeMX-6.8.0.sh", it was prompt:Check exe path on linux FullExe path1 is: /usr/bin/SetupSTM32CubeMX-6.8.0 Exe path is: /usr/bin Search java from relative path ---- Checking java in /usr/bin/./jre/bin/java Checking java in /usr/bin/.....

MQi.1 by Senior II
  • 11286 Views
  • 11 replies
  • 0 kudos

"Modified" column in GPIO configuration

Hello, what is meaning of the "Modified" column in GPIO configuration? When given pin is considered as modified? I am not able to find that information in CubeMX user manual...

_legacyfs_online_stmicro_images_0693W00000bjg2gQAA.png
MLaso by Associate II
  • 2427 Views
  • 2 replies
  • 0 kudos

NUCLEO-C031C6: Error when updating via MX

Good day,There seems to be an error in the implementation of the NUCLEO-C031C6 when generating code for the project after updating the peripherals. After loading an example project and compiling and testing all is well but once you update the project...

CKlib by Associate II
  • 4599 Views
  • 7 replies
  • 0 kudos

Resolved! CAN-Bus no callback/received frame; FDCAN STM32G473

I'm trying to attempt CAN on a STM32G473 MCU. While transmission seems to be fine, I'm not receiving any data back. The receive call back function is not triggering.Following is my setup:Below is the TxHeader and RxHeader initialization along with th...

_legacyfs_online_stmicro_images_0693W00000bjJuuQAE.png _legacyfs_online_stmicro_images_0693W00000bjJx0QAE.png
MMoha.10 by Associate III
  • 3118 Views
  • 2 replies
  • 0 kudos

Does Cube MX build the libc.a printf/canf/heap/etc library?

Yesterday's post herehttps://community.st.com/s/question/0D53W00002F4MHrSAN/is-there-a-bug-in-the-newlib-heap-on-the-32f417-cube-ide-library?t=1682872893044refers.This articlehttps://nadler.com/embedded/newlibAndFreeRTOS.htmlsuggests that the freerto...

PHolt.1 by Senior III
  • 7031 Views
  • 13 replies
  • 0 kudos

Can't install STMCUFinder on MacOS Ventura 13.3.

This is a prerequisite for the VSCode extension which is why I am asking here.Steps to reproduce:Download the setup filePer Readme.html, open a terminal, navigate to the en folder and run the following command: sudo xattr -cr ./SetupSTMCUFinder-5.0.0...

Resolved! STM32H755 Nucleo and PWR_DIRECT_SMPS_SUPPLY

Hi, I'm using an STM32H755ZIQ Nucleo and migrating an old project in CubeMX 6.8.The RCC > supply source > PWR_DIRECT_SMPS_SUPPLY option has been removed from CubeMX, which was the default previously. I tried the two available options (External / LDO...

MJack.1 by Associate III
  • 6000 Views
  • 6 replies
  • 1 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.