STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1757 Views
  • 0 replies
  • 2 kudos

Resolved! STM32G030K8T6 HSE Crystal Resonator Option Missing (CubeMX)?

Hello,I recently developed a board to use the STM32G030K8T6 under the assumption that it could support an external crystal oscillator (given what is said in the datasheet) and as I was setting it up in the CubeMX tool I noticed that the HSE was only ...

RGuin.3 by Associate
  • 4100 Views
  • 5 replies
  • 0 kudos

Resolved! STM32CubeMX doesn't generate the project well, it left MXTmpFiles when I build the configurations.

Hello.I'm using the lastest version of STM32CubeIDE, 1.12.1.The problem occurs after configuring al the STM32CubeMX perifereals and I try to build the project so it generates al the files that I need. But when I press the yellow wheel icon, the proje...

_legacyfs_online_stmicro_images_0693W00000bj3aBQAQ.png

Wrong USART3 pins on Nucleo-F756ZG

Hi,On my Nucleo-F756ZG, when I generate code for USART3 that's by default connected to ST-LINK , Cube sets pins for morpho connector (PB10 PB11) instead of alternate function (PD8 PD9). I also use Nucleo-L476RG and for this board, Cube set alternate ...

Resolved! Generate Single pulse using timer using HAL / CubeMx

I have been reading reading anything i could find on Timers, but I'm still confused about the setup in CubeMx.I just want to trigger a timer in software, that generates a SINGLE pulse with a set width (and if possible after a set dely) on a pin, but ...

RKage.3 by Associate
  • 9403 Views
  • 6 replies
  • 10 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.