2025-11-27 4:17 AM - last edited on 2025-11-27 4:30 AM by Andrew Neil
I have set XSPI1 to "Hexa SPI" mode. I'm using EXTMEM_MANAGER to manage the memory. I'm unable to select the setting EXTMEM_LINK_CONFIG_16LINE for "Number of memory data lines". Instead there is a info textbox which says "Active only when XSPI enabled in Hexa SPI mode.". The only available option is EXTMEM_LINK_CONFIG_1LINE. This results the EXTMEM_DRIVER_PSRAM_Init function to fail in the Config switch case, as the only options in the switch case are EXTMEM_LINK_CONFIG_16LINE and EXTMEM_LINK_CONFIG_8LINE.
If i manually force the Config to be EXTMEM_LINK_CONFIG_16LINE before the switch case, it seems to work.
I believe that i should be able to select EXTMEM_LINK_CONFIG_16LINE with MX if my XSPI is configured to Hexa SPI mode.
Solved! Go to Solution.
2026-02-25 3:17 AM
Hello @Tuomas95
This issue has been resolved in the latest version of STM32CubeMX 6.17.0
THX
Ghofrane
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2025-11-27 4:33 AM - edited 2025-11-27 6:07 AM
Hello @Tuomas95
Thanks for your valuable contribution.
Issue has been escalated to dev team under internal ticket ID 222668 and it will be fixed as soon as possible.
I will keep you posted with updates.
THX
Ghofrane
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2026-02-25 3:17 AM
Hello @Tuomas95
This issue has been resolved in the latest version of STM32CubeMX 6.17.0
THX
Ghofrane
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.