STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1756 Views
  • 0 replies
  • 2 kudos

Cannot get STM32MP157F-DK2 to recognize WiFi chip

I can't get my board to detect the WiFi chip over SDIO. I configured my boot SD card with a custom Linux install and everything is working except WiFi. It seems the WiFi chip is not recognized at all over the SDIO bus.  dir listing of /sys/bus/sdio/d...

CubeMX set files in read only mode on each generation

Hello,I'm working with STM32CubeMX version 6.9.2Each time I generate, all files in Drivers and in Middlewares\Third_Party\FreeRTOS directory are set in read only mode. I can remove it, and each time read only mode is set again.This is really annoying...

ANauz.1 by Senior II
  • 2833 Views
  • 3 replies
  • 0 kudos

CubeMX I2C stupid UX issue

Every time I need to configure I2C, which is not often, I have to check the correct rise and fall times for the default 100kHz frequency and doing so I am asking myself a question why the typical 100kHz value is provided by default but rise and fall ...

Screenshot 2023-09-15 214541.png
TDJ by Lead
  • 5711 Views
  • 11 replies
  • 0 kudos

Resolved! STM32CubeMX import pin-compatible STM32H7

Greetings,I'm having trouble porting the existing CubeMX configuration to a pinout compatible MCU.I'm using STM32H745IIK6 and trying to change it to STM32H755IIK6 following the instructions on page 287. of UM1718 Rev 34 ("Tutorial 5: Exporting curren...

0693W00000BajB5QAJ.png
DTomi.1 by Senior
  • 3375 Views
  • 4 replies
  • 0 kudos

Resolved! How can I have the STM32CubeMX Zigbee source files ?

Hello,I'm developping a Zigbee firmware for a custom board embedding a STM32WB MCU. So I'm using STM32CubeMX application to configure my card and the Zigbee middleware. For some reason, I need to understand how the differents Zigbee functions work an...

Evandzd by Associate
  • 2286 Views
  • 2 replies
  • 0 kudos

STM32CubeMX 6.9.2 released

STM32CubeMX 6.9.2 was released on st.com as well as an in-tool update patch. Main issues fixed in this patch: Ticket 158577 - [Bootpath Config] env.bat add quotes to variable stm32tpccliTicket 158868 - [Bootpath Config] secure manager post build cmd ...

Resolved! STM32H755bit getting stuck at WR_FLAG_VOSRDY

Hello,I have been working in a project with the mentioned MCU and by now i have been working it with SMPS_SUPPLY and VOS3 to work at 100Mhz Both CM7 and CM4.By now days i need to boost it up to 400Mhz and 200Mhz, so i need to change from VOS3 to VOS1...

urbito by Senior II
  • 4232 Views
  • 5 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.