STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1757 Views
  • 0 replies
  • 2 kudos

Resolved! CubeMX interface bug

I've been having problems with the CubeMX interface for quite some time now, starting 1-2 years before Windows 11 was released.The problem with the interface can appear both after 10-15 minutes of working in CubeMX and immediately after starting the ...

AndriikoM by Associate II
  • 6708 Views
  • 5 replies
  • 0 kudos

Resolved! CubeMX LoraWAN support

Is there any explanation to how to use production DevEUI, JoinEUI, AppKey and NetwKey, rather than the hardcoded se-identity.h?I have searched all over, application notes, youtube and even studied examples and the actual code, but unable to find out ...

Resolved! CubeMX / STM32H753IIKx / Clock Configuration

Hello,I have update a CubeMX project from V6.6.1 to V6.7.0.After update, without any changes, the clock configuration has a lot of errors. The CPU has a maximum clock rate from 480MHz, but the new CubeMX V6.7.0 allow only 200MHz!?!The Error:"D1CPRE C...

MMüll.6 by Associate III
  • 6400 Views
  • 7 replies
  • 0 kudos

How to add BSPs to code generated by STM32CUBEMX/IDE?

I'm currently having trouble adding BSPs my project using the STM32F769I-DISCO. After generating the code using STM32CUBEMX/IDE, I then downloaded the BSP file and copied and pasted it into the Drivers folders. I then manually added all the necessary...

0693W00000NqfUDQAZ.png 0693W00000NqfUXQAZ.png
JTurn.2 by Senior
  • 1630 Views
  • 1 replies
  • 1 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.