STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1756 Views
  • 0 replies
  • 2 kudos

Resolved! W25X20CL FLASH bring up with STM32H743 issue

Seeing issue while brining-up Winbond W25X20L FLASH with STM32, Write and read a byte in a loop does not work.Tried to see the signal's using the scope and seems like clock has some issue, appreciate any help. Please let mw know if more information i...

aahsan_1-1694645378744.png aahsan_0-1694644447709.png
aahsan by Associate III
  • 6258 Views
  • 7 replies
  • 2 kudos

Resolved! How to retarget printf on UART?

Hi All,I am new on STM32 and want to use printf on UART.I could run the printf on uart in the example folder.But couldnt find how does it work, actually couldnt find any comment in it about enabling printf on uart.I am useing STM32CubeMx and want to ...

MKora by Associate II
  • 6444 Views
  • 5 replies
  • 2 kudos

ai_platform.h file missing during analyze.

Hi, I'm getting "ai_platform.h" file missing when doing "analyze" under the X-CUBE-AI section.I was following the steps from a contest, I have followed the same steps on a different desktop computer and I didn't have this issue on that system. I don'...

Vishawjeet_Jyoti_0-1695841904871.png

Power-on startup Referenca Manual vs Cube-MX

Hallo, according to RM0433 6.4.1 "System supply startup" at point 5. "The software shall then initialize the system including supply configurationprogramming in PWR control register 3 (PWR_CR3). Once the supply configurationhas been configured, the A...

DrDro by Associate III
  • 1218 Views
  • 0 replies
  • 0 kudos

Resolved! Conflicting pins when using ADC

Hello. I examined similar questions and answers. Since I'm a newbie, I couldn't find an answer to my problem.In the documentation of the STM32F756ZG development board, it is said that up to 24 channels of ADC measurements can be usable with 3 ADCs. W...

picture1.png pict2.png
4embed by Associate
  • 6037 Views
  • 2 replies
  • 2 kudos

Resolved! STM32H743bi - use FDCAN2 and USB ULPI simultaneously?

Hello,I am using Cube32MX for STM32H743bi IO multiplexing. first i added USB HS phy ULPI interface then see FDCAN2 not allowed in the tool and error message says it is in conflict with USB ULPI. However i manually checked there were certain pins for ...

HKhan.1 by Associate II
  • 3943 Views
  • 5 replies
  • 0 kudos

Resolved! Simplest possible CubeMX USB app fails to enumerate

Posted on October 20, 2017 at 07:13 I have a brand-new STM32F303 Nucleo144 and cannot get any CubeMX generated apps to work with USB. The app builds and runs fine, and I can see printf output via SWO, but the device never evenbegins enumeration. Th...

Possible error in LCD configuration (wrong segment numbers)

HelloIn glass LCD display configuration (for STM32L152RB in my case), for static display, in Cube we can see segment numbers SEG[0-31]. Meanwhile, SEG[31:28] are double numbered, also to SEG[43:40]. To use [31:28] designators there must be MUX_SEG bi...

KDwor.17 by Associate
  • 1977 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.