STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1756 Views
  • 0 replies
  • 2 kudos

Hard Fault after call to static library

I'm using a BSEC static library for BME688 sensor. My application project builds fine. As soon as I reach the first BSEC function (which is provided by the "libalgobsec.a" static library), program goes to hard fault interrupt handler.My best guess wo...

lgacnik97 by Associate III
  • 2643 Views
  • 2 replies
  • 0 kudos

HAL_UARTEx_ReceiveToIdle_DMA repeating same data

I am currently using HAL_UARTEx_ReceiveToIdle_DMA and getting results that don't make sense to me. My main function is very simple: int main() { MX_DMA_Init(); MX_UART4_Init(); HAL_UARTEx_ReceiveToIdle_DMA(&huart4, rxDmaBuffer, sizeof(r...

aweav1 by Associate
  • 1748 Views
  • 1 replies
  • 0 kudos

Resolved! Problem with FreeRtos

Hi We are using product STM32H56 series , I am encountering problem while building my project .I am STM32cubeIDE , trust zone enabled .I enabled X-CUBE-FREERTOS  M33non secureIn software package I installed   -STm X-CUBE-FREERTOS  -CMSIS RTOS2-TZ_non...

Kendall7_0-1711443563549.png
Kendall7 by Associate II
  • 1659 Views
  • 1 replies
  • 0 kudos

UART Emulation AN4457 - is it possible to use it via CubeMx?

Hello,i was looking for some library to simulate UART on STM32 F4 MCU and i came across Application note AN4457. The note is clear in explaining how STSW-STM32156 firmware package provide such emulation and it looked really perfect for my case. Probl...

FCamp.1 by Associate III
  • 2028 Views
  • 3 replies
  • 1 kudos

Resolved! How the ADC works in F103RC

I've been confused for days and am unable to make the ADC work on F103RC and have to seek for help.The test consists of ADC1 with 6 channels, an UART for printf and an I/O port that drives an LED. The ADC configuration: The test code: /* USER CODE BE...

Chao_0-1711202637902.png Chao_2-1711202730095.png Chao_1-1711202678933.png Chao_3-1711202780449.png
Chao by Senior II
  • 6353 Views
  • 15 replies
  • 1 kudos

STM32H7 USB Dual Role: have Cube act as both host and device

Hello,I am trying to use an H7 with USB OTG as host/device. Only 1 will be enabled at any given time. The issue is that with Cube, if I set the FS PHY to OTG/Dual_Role_Device, I get nothing but the IO set. Which is, obviously, the opposite of what I ...

DShekter by Associate III
  • 3466 Views
  • 3 replies
  • 4 kudos

Resolved! ADC multichannel with DMA with more than 8 ADC channel

HI everybody,i am using STM32G0B1 and in an older project i used successful ADC multichannel DMA conversion of 8 channel. I started a multichannel ADC conversion of 8 channel and a ADC callbacksets the finished bit and later on i read the result for ...

Kai4_0-1710151106760.png
Kai4 by Associate II
  • 3495 Views
  • 3 replies
  • 1 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.