2024-03-14 12:40 AM
I have installed STM32CubeMX version 6.10.0 in Ubuntu 22.04 (through Windows Subsystem for Linux 2), but when I start it and click "INSTALL/REMOVE" to install the X-CUBE-AI extension, I get the following error message and nothing more happens:
[ERROR] CheckServerUpdateThread:123 - Unexpected exception CheckServer ThreadCannot invoke "com.teamdev.jxbrowser.browser.Browser.mainFrame()" because "this.browser" is null
I have tried manually installing Chromium and restarted the system after that, but I still get the same error.
How can I get the installation procedure to work?
2024-03-14 3:59 AM
Hello @magnus_lindhe ,
First let me thank you for posting.
This issue is under investigation, and I will get back to you as soon as possible.
Thanks.
Mahmoud.
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2024-03-27 2:19 AM
Hello @magnus_lindhe ,
The issue was not reproduced. The installation of X-Cube-AI extension was successful using STM32CubeMX 6.10.0 and Ubuntu 22.04.
I suggest that you download the package from this link X-CUBE-AI - AI expansion pack for STM32CubeMX - STMicroelectronics and load it manually.
Thanks.
Mahmoud.
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.