STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1756 Views
  • 0 replies
  • 2 kudos

Resolved! USART3 not available to use in CubeMX

I am trying to generate code using CubeMX (version 6.11.1), using the NUCLEO-H563ZI board to start the project. But, I am getting the following pop-up when trying to use the USART3 peripheral which seems to be unavailable:Because of this, I had to do...

AShetty_0-1723109965194.png AShetty_1-1723110323714.png
AShetty by Associate II
  • 4002 Views
  • 7 replies
  • 6 kudos

The signal result becomes a straight line on the DAC

 "I am using your program and made some changes, but when I use it in the function  HAL_DAC_Start_DMA(&hdac, DAC_CHANNEL_1, (uint32_t*)value, 89, DAC_ALIGN_12B_R); HAL_TIM_Base_Start(&htim4); the signal result on the oscilloscope is not continuous. ...

WhatsApp Image 2024-09-06 at 16.06.24 (1).jpeg WhatsApp Image 2024-09-06 at 16.06.24.jpeg
macam1 by Associate III
  • 2762 Views
  • 7 replies
  • 0 kudos

Resolved! How do I make stm32 and w25q128 work as a usb msc?

I am trying to use stm32f407 and w25q128 to get a usb drive, for this I wrote a driver to control the flash drive and initialized the USB MSC using CubeMX. When I connect the stm32 to the PC (Ubuntu) I see the new storage device in the Disks app but ...

Resolved! How to get interrupt handler generated by CubeMX?

Hi guysI want to generate a time base by a general purpose timer interrupt (TIM6) on a F334 with low level library. I do not know why, I get init functions fine but no interrupt request handler is generated, nowhere.It should be very simple, I though...

White_Fox by Associate III
  • 2861 Views
  • 3 replies
  • 2 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.