STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1756 Views
  • 0 replies
  • 2 kudos

Resolved! Configuring PWM on stm32f405

Hi there;I'm extremely new to the world of ST, and trying to get my feet under me with it, coming from a few years' experience developing for esp32 microcontrollers using the esp-idf framework. I have an Adafruit stm32f405 feather; I understand this ...

Screen Shot 2024-09-15 at 7.47.40 PM.png
sb_st by Senior II
  • 5211 Views
  • 7 replies
  • 0 kudos

Resolved! CubeMX 6.11.1 removes LWIP part of H7 .ioc file

Hi there!Opening an H7.ioc file FW_H7 V1.11.1 in CubeMX 6.11.1 containing a LWIP secition and upgrade to FW_H7 V1.11.2 removes LWIP section.Cheers!open the attached .ioc file in CubeMX 6.11.1migrate to FW version FW_H7 V1.11.2do not change anything a...

PGrif2_1-1716908478187.png PGrif2_0-1716908294052.png PGrif2_2-1716908610818.png
PGrif.2 by Associate III
  • 2077 Views
  • 2 replies
  • 0 kudos

ThreadX systick code generation

For my project I'm using an STM32L476 MCU with CubeIDE 1.15.1 and CubeMX 6.11.1In this project I'm using ThreadX / Azure RTOS.For a new feature I doubled the speed of the MSI, which doubles the system clock, but the HCLK stays the same (by changing t...

EmbDev by Senior
  • 4190 Views
  • 6 replies
  • 1 kudos

Resolved! issue with FW_V1.10.0 not pinging in stm32h743

im using stm32h743zi2 nucleo board . im triyng to do programming in ethernet with udp without freeRTOS . using firmware version of 1.10.0 but it is not pinging .  anybody  did programming with this FW  . please let me know the reasons for not ping.or...

STm32H563 RS485 DE-Configuration in CubeIDE

Hello,in CubeIDE (MX) RS485-direction switching is only selectable for UART4 and UART5 (by hardware, not by SW-GPIO). According to user manual, it should be possible for all UARTs/USARTs (Pin DE/RTS). Is this feature missing in CubeIDE or is this har...

pit0815 by Associate
  • 3435 Views
  • 5 replies
  • 0 kudos

Resolved! MXCUBE USART on H7S3

HI Forum,I am configuring my USART as a synchronous slave receive only, the cube software configures clock, receive and transmit GPIO and I cannot remove the transmit GPIO configuration in the GUI without it removing the entire peripheral.  Is their ...

gvigelet by Associate II
  • 3089 Views
  • 3 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.