2024-08-15 5:34 AM
My platform is Windows 11. I had to run STM32CubeMX in a command-line mode. According to the video tutorial and UM1718:
jre\bin\java -jar STM32CubeMX.exe -i
runs STM32CubeMX in interactive command-line mode.
It took me a long time to find out that it works only if I append a Project.ioc. Otherwise, the cursor is not in the desired MX> position. My apologies if this happens only in my case. If it is common, I expect ST to exhibit more maturity in providing documentation.
2024-09-07 4:26 PM
Hello @golvict
It is mentionned on the UM1718 that you have to use the STM32CubeMX installation path before executing the run command.
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2024-09-07 5:13 PM
Confirmed. If no .ioc file is specified after -i then MX> prompt is not displayed. But MX is in command mode. You can type a command, for example 'help' and it will be executed and then prompt MX> is displayed.
#DoNotPanic
2024-09-07 5:40 PM
Thank you so much @Pavel A. . I will escalate it internaly for more clarifications on the comming versions.
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.