STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1756 Views
  • 0 replies
  • 2 kudos

Resolved! Cannot download CubeMX, CubeIDE, CubeProgrammer

Hello Everyone,I have read several posts on this forum for the same problem that I am posting.I cannot download CubeMX, CubeIDE, CubeProgrammer from the Developer zone.I have tried several browsers (Firefox, Brave).I have tried 2 desktop computers (H...

xst by Associate III
  • 4840 Views
  • 8 replies
  • 6 kudos

How to execute ENTDAA multiple times

When executing RSTDAA and ENTDAA once, it succeeds, but when executed more than twice, it does not work properly. Since RSTDAA is being performed, I think there should be no problem, but is it not possible to execute it more than twice?//1st rstdaa+e...

dai82s by Associate II
  • 994 Views
  • 0 replies
  • 0 kudos

Resolved! VREFBUF not available

I have an STM32U535RET6 chipset and I'm trying to enable it's voltage reference buffer, but I can't. I have the latest version of the STM32 Cube IDE, and I'm stuck at the "VREF+ is double bonded with VDDA in this package" message. What's interesting ...

PXL_20240918_122735513.MP.jpg Zer0_1-1726724982322.png
Zer0 by Associate II
  • 3043 Views
  • 6 replies
  • 5 kudos

Resolved! Input Capture Interrupt on TIM4

Hi,Id need to measure the frequency of an input signal using TIM4. My device is a STM32L475RCT and to do this I've used the TIM_InputCapture example from CubeIDE. In my application TIM1 is not available.The problem is for the TIM4 I'm not able to set...

0693W00000AQ8wyQAD.png
Gaston by Senior
  • 5518 Views
  • 6 replies
  • 0 kudos

stm32cubemx cmake code generation

I've been using the recently added CMake generation feature of cubemx, as of now it creates an INTERFACE library for both project related and drivers related sources, the problem is that those sources get propagated for every external library that ne...

Tizio1234 by Associate II
  • 3309 Views
  • 2 replies
  • 1 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.