2024-10-24 7:18 PM
Hi,
I have setup and configured an STM32H5-based MCU via STM32CubeMX and with cmake as build system.
I managed to build it successfully using Ninja generator. However, I can't change the configuration to Release and it is always Debug even though I used -DCMAKE_BUILD_TYPE=Release.
I tried this in command line and using STM32 VSCODE Extension and all with the same results.
I even tried to pass -DCMAKE_CONFIGURATION_TYPES="Debug;Release".
Here is my build script:
@echo off
set TargetBuild=%1
:CHECK_INPUT
IF [%TargetBuild%] == [] GOTO :ERROR
:PROCESS
cd ../ &
rm -rf Secure/build &
rm -rf NonSecure/build &
rm -rf build
mkdir build &
cd build &
cmake -DCMAKE_CONFIGURATION_TYPES=%TargetBuild% -DCMAKE_BUILD_TYPE=%TargetBuild% -DCMAKE_TOOLCHAIN_FILE=gcc-arm-none-eabi.cmake -B%TargetBuild% -G Ninja -S../ &
cd %TargetBuild% &
ninja
goto :eof
:ERROR
echo "Error: No target build given"
echo "Usage Example:""
echo "_build.cmd Release"
goto :eof
2024-10-25 1:05 AM
Hello @hakeila
Before reconfiguring, make sure to clean any previous build artifacts. You can do this by removing the build directory entirely:
rm -rf build
mkdir build
cd build
Visual Studio Code Settings:
If you're using Visual Studio Code with the STM32 extension, ensure that your tasks and launch configurations are set up correctly to reflect the desired build type.
Example Build Script Adjustment
Here’s a refined version of your batch script that includes checks and ensures proper handling of the build type:
@echo off
set TargetBuild=%1
:CHECK_INPUT
IF [%TargetBuild%] == [] GOTO :ERROR
:PROCESS
cd ..\ &
rm -rf Secure\build & rm -rf NonSecure\build & rm -rf build
mkdir build & cd build &
cmake -DCMAKE_CONFIGURATION_TYPES="%TargetBuild%" -DCMAKE_BUILD_TYPE="%TargetBuild%" -DCMAKE_TOOLCHAIN_FILE=gcc-arm-none-eabi.cmake -G Ninja -S .. &
cd %TargetBuild% & ninja
goto :eof
:ERROR
echo "Error: No target build given"
echo "Usage Example:"
echo "_build.cmd Release"
goto :eof
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2024-10-28 1:58 PM - edited 2024-10-28 8:50 PM
Hi Ghofrane,
Thank you so much reply.
I actually tried your suggestion and copied your refined version of the script. I also made sure that my build starts with a clean build. But the generated build is always set at debug. Here is the CMake output:
Generated with config types: Release
-- The C compiler identification is GNU 12.3.1
-- The CXX compiler identification is GNU 12.3.1
Build context: Secure
Build context: NonSecure
-- Configuring done (2.2s)
-- Generating done (0.0s)
-- Build files have been written to: C:/Users/hakeila/projects/WxplNG/build
[1/1] Cleaning all built files...
Cleaning... 0 files.
[5/16] Performing configure step for 'WxplNG_S'
Build type: Debug
-- The C compiler identification is GNU 12.3.1
-- The CXX compiler identification is GNU 12.3.1
-- The ASM compiler identification is GNU
-- Found assembler: C:/ST/STM32CubeCLT_1.16.0/GNU-tools-for-STM32/bin/arm-none-eabi-gcc.exe
-- Configuring done (2.4s)
-- Generating done (0.0s)
-- Build files have been written to: C:/Users/hakeila/projects/WxplNG/Secure/build
[6/16] Performing build step for 'WxplNG_S'
[1/25] Building C object CMakeFiles/WxplNG_S.dir/Src/icache.c.obj
[2/25] Building C object CMakeFiles/WxplNG_S.dir/Src/main.c.obj
[3/25] Building C object CMakeFiles/WxplNG_S.dir/Src/stm32h5xx_it.c.obj
[4/25] Building C object CMakeFiles/WxplNG_S.dir/Src/gtzc_s.c.obj
[5/25] Building C object CMakeFiles/WxplNG_S.dir/Src/stm32h5xx_hal_msp.c.obj
[6/25] Building C object CMakeFiles/WxplNG_S.dir/C_/Users/hakeila/projects/WxplNG/Drivers/STM32H5xx_HAL_Driver/Src/stm32h5xx_hal_rcc.c.obj
[7/25] Building C object CMakeFiles/WxplNG_S.dir/C_/Users/hakeila/projects/WxplNG/Drivers/STM32H5xx_HAL_Driver/Src/stm32h5xx_hal_cortex.c.obj
[8/25] Building C object CMakeFiles/WxplNG_S.dir/Src/secure_nsc.c.obj
[9/25] Building C object CMakeFiles/WxplNG_S.dir/C_/Users/hakeila/projects/WxplNG/Drivers/STM32H5xx_HAL_Driver/Src/stm32h5xx_hal_gtzc.c.obj
[10/25] Building C object CMakeFiles/WxplNG_S.dir/C_/Users/hakeila/projects/WxplNG/Drivers/STM32H5xx_HAL_Driver/Src/stm32h5xx_hal_rcc_ex.c.obj
[11/25] Building C object CMakeFiles/WxplNG_S.dir/C_/Users/hakeila/projects/WxplNG/Drivers/STM32H5xx_HAL_Driver/Src/stm32h5xx_hal_flash.c.obj
[12/25] Building C object CMakeFiles/WxplNG_S.dir/C_/Users/hakeila/projects/WxplNG/Drivers/STM32H5xx_HAL_Driver/Src/stm32h5xx_hal_flash_ex.c.obj
[13/25] Building C object CMakeFiles/WxplNG_S.dir/C_/Users/hakeila/projects/WxplNG/Drivers/STM32H5xx_HAL_Driver/Src/stm32h5xx_hal_gpio.c.obj
[14/25] Building C object CMakeFiles/WxplNG_S.dir/C_/Users/hakeila/projects/WxplNG/Drivers/STM32H5xx_HAL_Driver/Src/stm32h5xx_hal_pwr.c.obj
[15/25] Building C object CMakeFiles/WxplNG_S.dir/C_/Users/hakeila/projects/WxplNG/Drivers/STM32H5xx_HAL_Driver/Src/stm32h5xx_hal_dma.c.obj
[16/25] Building C object CMakeFiles/WxplNG_S.dir/C_/Users/hakeila/projects/WxplNG/Drivers/STM32H5xx_HAL_Driver/Src/stm32h5xx_hal_icache.c.obj
[17/25] Building C object CMakeFiles/WxplNG_S.dir/C_/Users/hakeila/projects/WxplNG/Drivers/STM32H5xx_HAL_Driver/Src/stm32h5xx_hal.c.obj
[18/25] Building C object CMakeFiles/WxplNG_S.dir/C_/Users/hakeila/projects/WxplNG/Drivers/STM32H5xx_HAL_Driver/Src/stm32h5xx_hal_exti.c.obj
[19/25] Building C object CMakeFiles/WxplNG_S.dir/C_/Users/hakeila/projects/WxplNG/Drivers/STM32H5xx_HAL_Driver/Src/stm32h5xx_hal_pwr_ex.c.obj
[20/25] Building C object CMakeFiles/WxplNG_S.dir/Src/sysmem.c.obj
[21/25] Building ASM object CMakeFiles/WxplNG_S.dir/startup/startup_stm32h523xx.s.obj
[22/25] Building C object CMakeFiles/WxplNG_S.dir/C_/Users/hakeila/projects/WxplNG/Drivers/STM32H5xx_HAL_Driver/Src/stm32h5xx_hal_dma_ex.c.obj
[23/25] Building C object CMakeFiles/WxplNG_S.dir/Src/syscalls.c.obj
[24/25] Building C object CMakeFiles/WxplNG_S.dir/Src/system_stm32h5xx_s.c.obj
[25/25] Linking C executable WxplNG_S.elf
Memory region Used Size Region Size %age Used
RAM: 1592 B 208 KB 0.75%
FLASH: 6028 B 248 KB 2.37%
FLASH_NSC: 32 B 8 KB 0.39%
[13/16] Performing configure step for 'WxplNG_NS'
Build type: Debug
-- The C compiler identification is GNU 12.3.1
-- The CXX compiler identification is GNU 12.3.1
-- The ASM compiler identification is GNU
-- Found assembler: C:/ST/STM32CubeCLT_1.16.0/GNU-tools-for-STM32/bin/arm-none-eabi-gcc.exe
-- Configuring done (2.2s)
-- Generating done (0.0s)
-- Build files have been written to: C:/Users/hakeila/projects/WxplNG/NonSecure/build
[14/16] Performing build step for 'WxplNG_NS'
[1/22] Building C object CMakeFiles/WxplNG_NS.dir/Src/main.c.obj
[2/22] Building C object CMakeFiles/WxplNG_NS.dir/C_/Users/hakeila/projects/WxplNG/Drivers/STM32H5xx_HAL_Driver/Src/stm32h5xx_hal_flash.c.obj
[3/22] Building C object CMakeFiles/WxplNG_NS.dir/Src/stm32h5xx_it.c.obj
[4/22] Building C object CMakeFiles/WxplNG_NS.dir/C_/Users/hakeila/projects/WxplNG/Drivers/STM32H5xx_HAL_Driver/Src/stm32h5xx_hal_cortex.c.obj
[5/22] Building C object CMakeFiles/WxplNG_NS.dir/C_/Users/hakeila/projects/WxplNG/Drivers/STM32H5xx_HAL_Driver/Src/stm32h5xx_hal_gpio.c.obj
[6/22] Building C object CMakeFiles/WxplNG_NS.dir/Src/stm32h5xx_hal_msp.c.obj
[7/22] Building C object CMakeFiles/WxplNG_NS.dir/C_/Users/hakeila/projects/WxplNG/Drivers/STM32H5xx_HAL_Driver/Src/stm32h5xx_hal_flash_ex.c.obj
[8/22] Building C object CMakeFiles/WxplNG_NS.dir/C_/Users/hakeila/projects/WxplNG/Drivers/STM32H5xx_HAL_Driver/Src/stm32h5xx_hal_rcc.c.obj
C:/Users/hakeila/projects/WxplNG/Drivers/STM32H5xx_HAL_Driver/Src/stm32h5xx_hal_rcc.c: In function 'HAL_RCC_ConfigAttributes':
C:/Users/hakeila/projects/WxplNG/Drivers/STM32H5xx_HAL_Driver/Src/stm32h5xx_hal_rcc.c:1754:40: warning: unused parameter 'Item' [-Wunused-parameter]
1754 | void HAL_RCC_ConfigAttributes(uint32_t Item, uint32_t Attributes)
| ~~~~~~~~~^~~~
C:/Users/hakeila/projects/WxplNG/Drivers/STM32H5xx_HAL_Driver/Src/stm32h5xx_hal_rcc.c: In function 'HAL_RCC_GetConfigAttributes':
C:/Users/hakeila/projects/WxplNG/Drivers/STM32H5xx_HAL_Driver/Src/stm32h5xx_hal_rcc.c:1834:56: warning: unused parameter 'Item' [-Wunused-parameter]
1834 | HAL_StatusTypeDef HAL_RCC_GetConfigAttributes(uint32_t Item, uint32_t *pAttributes)
| ~~~~~~~~~^~~~
[9/22] Building C object CMakeFiles/WxplNG_NS.dir/C_/Users/hakeila/projects/WxplNG/Drivers/STM32H5xx_HAL_Driver/Src/stm32h5xx_hal_dma.c.obj
[10/22] Building C object CMakeFiles/WxplNG_NS.dir/C_/Users/hakeila/projects/WxplNG/Drivers/STM32H5xx_HAL_Driver/Src/stm32h5xx_hal_rcc_ex.c.obj
[11/22] Building C object CMakeFiles/WxplNG_NS.dir/Src/syscalls.c.obj
[12/22] Building C object CMakeFiles/WxplNG_NS.dir/C_/Users/hakeila/projects/WxplNG/Drivers/STM32H5xx_HAL_Driver/Src/stm32h5xx_hal_pwr.c.obj
C:/Users/hakeila/projects/WxplNG/Drivers/STM32H5xx_HAL_Driver/Src/stm32h5xx_hal_pwr.c: In function 'HAL_PWR_ConfigAttributes':
C:/Users/hakeila/projects/WxplNG/Drivers/STM32H5xx_HAL_Driver/Src/stm32h5xx_hal_pwr.c:527:40: warning: unused parameter 'Item' [-Wunused-parameter]
527 | void HAL_PWR_ConfigAttributes(uint32_t Item, uint32_t Attributes)
| ~~~~~~~~~^~~~
C:/Users/hakeila/projects/WxplNG/Drivers/STM32H5xx_HAL_Driver/Src/stm32h5xx_hal_pwr.c: In function 'HAL_PWR_GetConfigAttributes':
C:/Users/hakeila/projects/WxplNG/Drivers/STM32H5xx_HAL_Driver/Src/stm32h5xx_hal_pwr.c:610:56: warning: unused parameter 'Item' [-Wunused-parameter]
610 | HAL_StatusTypeDef HAL_PWR_GetConfigAttributes(uint32_t Item, uint32_t *pAttributes)
| ~~~~~~~~~^~~~
[13/22] Building C object CMakeFiles/WxplNG_NS.dir/Src/sysmem.c.obj
[14/22] Building C object CMakeFiles/WxplNG_NS.dir/C_/Users/hakeila/projects/WxplNG/Drivers/STM32H5xx_HAL_Driver/Src/stm32h5xx_hal_pwr_ex.c.obj
[15/22] Building C object CMakeFiles/WxplNG_NS.dir/C_/Users/hakeila/projects/WxplNG/Drivers/STM32H5xx_HAL_Driver/Src/stm32h5xx_hal_tim.c.obj
[16/22] Building C object CMakeFiles/WxplNG_NS.dir/C_/Users/hakeila/projects/WxplNG/Drivers/STM32H5xx_HAL_Driver/Src/stm32h5xx_hal_tim_ex.c.obj
[17/22] Building C object CMakeFiles/WxplNG_NS.dir/C_/Users/hakeila/projects/WxplNG/Drivers/STM32H5xx_HAL_Driver/Src/stm32h5xx_hal_exti.c.obj
[18/22] Building ASM object CMakeFiles/WxplNG_NS.dir/startup/startup_stm32h523xx.s.obj
[19/22] Building C object CMakeFiles/WxplNG_NS.dir/Src/system_stm32h5xx_ns.c.obj
[20/22] Building C object CMakeFiles/WxplNG_NS.dir/C_/Users/hakeila/projects/WxplNG/Drivers/STM32H5xx_HAL_Driver/Src/stm32h5xx_hal.c.obj
[21/22] Building C object CMakeFiles/WxplNG_NS.dir/C_/Users/hakeila/projects/WxplNG/Drivers/STM32H5xx_HAL_Driver/Src/stm32h5xx_hal_dma_ex.c.obj
[22/22] Linking C executable WxplNG_NS.elf
Memory region Used Size Region Size %age Used
RAM: 1584 B 64 KB 2.42%
FLASH: 5988 B 256 KB 2.28%
[16/16] Completed 'WxplNG_NS'
You can see the Build Type: Debug from the attached cmake output above.
the main CMakeLists.txt doesn't see my CMAKE_BUILD_TYPE variable and thus it set it to debug.
I even tried to set the CMAKE_BUILD_TYPE in STMCubeCX generated parent CMakeLists.txt with Release version, but the successive .cmake files don't see this variable.
2024-10-28 4:07 PM - edited 2024-10-28 8:51 PM
With more digging into this cmake issue, I found out that this system is considered as multi-configuration setting
I typed the CMAKE_BUILD_TYPE in the parent CMakeLists.txt and it was indeed a Release build but for some reason, this variable is not passed to the successive CMakeLists.txt in Secure and NonSecure sub-folders for some reason
I also made sure that the generated .ninja file does contain the build configuration as release
What is going wrong here?
2024-10-28 9:20 PM - edited 2024-10-30 2:52 PM
I managed to fix the issue but I had to manually modify the mx-generated.cmake file (which is automatically generated from STMCubeMX). I added -DCMAKE_BUILD_TYPE=${CMAKE_BUILD_TYPE} into the CMAKE_ARGS as shown in the attached mx-generated.cmake file.
I think the ExternalProject_Add() function in the original mx-generated.cmake has its own cmake args scope which made the CMAKE_BUILD_TYPE variable always null and thus, the successive CMakeLists.txt in Secure and NonSecure folders always set it to Debug due to failed if(NOT CMAKE_BUILD_TYPE) check
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.