STM32CubeMonitor (MCUs)

Ask questions on STM32CubeMonitor. Discuss the latest updates, including specialized versions (power, RF, USB-PD).

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMonitor-1.12.0 is available

Hello The version 1.12.0 of STM32CubeMonitor is available on st.com :  https://www.st.com/en/development-tools/stm32cubemonitor.html What are the main changes in this version ? Node-RED® updated to version 4.1.3.STM32 devices list updated.Software de...

STM32CubeMonitor-RF V2.19.0 is available

Hello A new release of STM32CubeMonitor-RF is available on st.com. Click on "Get latest" to download the version 2.19.0. What are the main changes in this version ? Alignment with STM32CubeWB firmware 1.24.0.Alignment with STM32CubeWBA firmware 1.8.0...

STM32 Cube Monitor not able to parse ELF file

Hello,Currently I am facing a issue where my CUBE monitor is not able to parse the ELF files. It gets stuck at 10% completion while loading it. I have attached my workflow below:The Error is as follows:   It will be very helpful if anyone can provide...

Screenshot 2025-08-11 130120.png Screenshot 2025-08-11 131018.png Prishat_0-1754898076764.png
Prishat by Associate
  • 1138 Views
  • 4 replies
  • 0 kudos

Installation of STM32CubeMonitor on Manjaro

I installed Manjaro Linux, downloaded STM32CubeMonitor from the official website, and then installed it via yay by replacing the package’s cached file with the official one:rm -rf .cache/yay/stm32cubemonitor/en.stm32cubemon-lin-v-1-10-0.zipmv stm32cu...

Oz1_0-1753771901106.png
Oz1 by Associate
  • 3217 Views
  • 2 replies
  • 0 kudos

how can i use daplink in stm32cubemonitor

For well-known reasons, I'm developing on STM32F4 using DAPLink, but encountered an issue when trying to track analog signal variations with STM32CubeMonitor. CubeMonitor seems unable to detect DAPLink. Is there any solution to resolve this problem?

STM32CubeMonitor .elf issue

Hello, I want to use STM32CubeMonitor to debug the code. The .elf is imported into CubeMonitor, and the connection is built. However, clicking on "Deploy", the follow error message shows: "TypeError: Cannot read properties of null (reading 'variablel...

STuser100 by Associate II
  • 1312 Views
  • 1 replies
  • 0 kudos