2025-12-10 5:05 AM
I have a characteristic that supports write and indicate. A command is written to the char, the server responds by indicating the characteristic to the client.
I'm using Stm32CubeMonitor-RF 2.19.0 to test the server, but indications always cause a ACI_GATT_PROC_TIMEOUT_EVENT because STM32CubeMonitor-RF does not issue a ACI_GATT_CONFIRM_INDICATION after an indication is received.
log file attached.
2025-12-10 7:45 AM
Thank you for reporting, unfortunately, your log could not be read for the moment see this post.
2025-12-10 8:59 AM
log file:
Nb,Time,Port Com,Type,Parameter,Value,Literal,Information
1328,13:56:41:283,COM6,ACI_GATT_WRITE_CHAR_VALUE,hci_packet_indicator,0x01,HCI Command Packet,
1328,13:56:41:283,COM6,ACI_GATT_WRITE_CHAR_VALUE,op_code,0xFD1C,ACI_GATT_WRITE_CHAR_VALUE,
1328,13:56:41:283,COM6,ACI_GATT_WRITE_CHAR_VALUE,parameter_total_length,0x06,,
1328,13:56:41:283,COM6,ACI_GATT_WRITE_CHAR_VALUE,connection_handle,0x0801,,Specifies the ATT bearer for which the command applies.. Possible values:. 0x0000 ... 0x0EFF: Unenhanced ATT bearer (the parameter is the connection handle). 0xEA00 ... 0xEA3F: Enhanced ATT bearer (the LSB-byte of the parameter is the connection-oriented channel index)
1328,13:56:41:283,COM6,ACI_GATT_WRITE_CHAR_VALUE,attr_handle,0x0019,,Handle of the characteristic value to be written
1328,13:56:41:283,COM6,ACI_GATT_WRITE_CHAR_VALUE,attribute_val_length,0x01,,Length of the value to be written
1328,13:56:41:283,COM6,ACI_GATT_WRITE_CHAR_VALUE,attribute_val,0x02,,Value to be written
1328,13:56:41:283,COM6,ACI_GATT_WRITE_CHAR_VALUE,Raw,[0x01:0x1C:0xFD:0x06:0x01:0x08:0x19:0x00:0x01:0x02],,
1329,13:56:41:284,COM6,HCI_COMMAND_STATUS_EVENT,hci_packet_indicator,0x04,HCI Event packet,
1329,13:56:41:284,COM6,HCI_COMMAND_STATUS_EVENT,event_code,0x0F,HCI_COMMAND_STATUS_EVENT,
1329,13:56:41:284,COM6,HCI_COMMAND_STATUS_EVENT,parameter_total_length,0x04,,
1329,13:56:41:284,COM6,HCI_COMMAND_STATUS_EVENT,status,0x00,Success,Status error code.
1329,13:56:41:284,COM6,HCI_COMMAND_STATUS_EVENT,num_hci_command_packets,0x01,,The Number of HCI command packets which are allowed to be sent to the Controller from the Host.
1329,13:56:41:284,COM6,HCI_COMMAND_STATUS_EVENT,command_opcode,0xFD1C,ACI_GATT_WRITE_CHAR_VALUE,Opcode of the command which caused this event.
1329,13:56:41:284,COM6,HCI_COMMAND_STATUS_EVENT,Raw,[0x04:0x0F:0x04:0x00:0x01:0x1C:0xFD],,
1330,13:56:41:435,COM6,HCI_VENDOR_EVENT,hci_packet_indicator,0x04,HCI Event packet,
1330,13:56:41:435,COM6,HCI_VENDOR_EVENT,event_code,0xFF,HCI_VENDOR_EVENT,
1330,13:56:41:435,COM6,HCI_VENDOR_EVENT,parameter_total_length,0x05,,
1330,13:56:41:435,COM6,HCI_VENDOR_EVENT,ecode,0x0C10,ACI_GATT_PROC_COMPLETE_EVENT,
1330,13:56:41:435,COM6,HCI_VENDOR_EVENT,connection_handle,0x0801,,Specifies the ATT bearer for which the event applies.. Possible values:. 0x0000 ... 0x0EFF: Unenhanced ATT bearer (the parameter is the connection handle). 0xEA00 ... 0xEA3F: Enhanced ATT bearer (the LSB-byte of the parameter is the connection-oriented channel index)
1330,13:56:41:435,COM6,HCI_VENDOR_EVENT,error_code,0x00,,"Indicates whether the procedure completed with an error or was successful (see ""Status error codes"" section)"
1330,13:56:41:435,COM6,HCI_VENDOR_EVENT,Raw,[0x04:0xFF:0x05:0x10:0x0C:0x01:0x08:0x00],,
1331,13:56:46:032,COM6,ACI_GATT_WRITE_CHAR_VALUE,hci_packet_indicator,0x01,HCI Command Packet,
1331,13:56:46:032,COM6,ACI_GATT_WRITE_CHAR_VALUE,op_code,0xFD1C,ACI_GATT_WRITE_CHAR_VALUE,
1331,13:56:46:032,COM6,ACI_GATT_WRITE_CHAR_VALUE,parameter_total_length,0x07,,
1331,13:56:46:032,COM6,ACI_GATT_WRITE_CHAR_VALUE,connection_handle,0x0801,,Specifies the ATT bearer for which the command applies.. Possible values:. 0x0000 ... 0x0EFF: Unenhanced ATT bearer (the parameter is the connection handle). 0xEA00 ... 0xEA3F: Enhanced ATT bearer (the LSB-byte of the parameter is the connection-oriented channel index)
1331,13:56:46:032,COM6,ACI_GATT_WRITE_CHAR_VALUE,attr_handle,0x0018,,Handle of the characteristic value to be written
1331,13:56:46:032,COM6,ACI_GATT_WRITE_CHAR_VALUE,attribute_val_length,0x02,,Length of the value to be written
1331,13:56:46:032,COM6,ACI_GATT_WRITE_CHAR_VALUE,attribute_val,0x0104,,Value to be written
1331,13:56:46:032,COM6,ACI_GATT_WRITE_CHAR_VALUE,Raw,[0x01:0x1C:0xFD:0x07:0x01:0x08:0x18:0x00:0x02:0x04:0x01],,
1332,13:56:46:033,COM6,HCI_COMMAND_STATUS_EVENT,hci_packet_indicator,0x04,HCI Event packet,
1332,13:56:46:033,COM6,HCI_COMMAND_STATUS_EVENT,event_code,0x0F,HCI_COMMAND_STATUS_EVENT,
1332,13:56:46:033,COM6,HCI_COMMAND_STATUS_EVENT,parameter_total_length,0x04,,
1332,13:56:46:033,COM6,HCI_COMMAND_STATUS_EVENT,status,0x00,Success,Status error code.
1332,13:56:46:033,COM6,HCI_COMMAND_STATUS_EVENT,num_hci_command_packets,0x01,,The Number of HCI command packets which are allowed to be sent to the Controller from the Host.
1332,13:56:46:033,COM6,HCI_COMMAND_STATUS_EVENT,command_opcode,0xFD1C,ACI_GATT_WRITE_CHAR_VALUE,Opcode of the command which caused this event.
1332,13:56:46:033,COM6,HCI_COMMAND_STATUS_EVENT,Raw,[0x04:0x0F:0x04:0x00:0x01:0x1C:0xFD],,
1333,13:56:46:155,COM6,HCI_VENDOR_EVENT,hci_packet_indicator,0x04,HCI Event packet,
1333,13:56:46:155,COM6,HCI_VENDOR_EVENT,event_code,0xFF,HCI_VENDOR_EVENT,
1333,13:56:46:155,COM6,HCI_VENDOR_EVENT,parameter_total_length,0x05,,
1333,13:56:46:155,COM6,HCI_VENDOR_EVENT,ecode,0x0C10,ACI_GATT_PROC_COMPLETE_EVENT,
1333,13:56:46:155,COM6,HCI_VENDOR_EVENT,connection_handle,0x0801,,Specifies the ATT bearer for which the event applies.. Possible values:. 0x0000 ... 0x0EFF: Unenhanced ATT bearer (the parameter is the connection handle). 0xEA00 ... 0xEA3F: Enhanced ATT bearer (the LSB-byte of the parameter is the connection-oriented channel index)
1333,13:56:46:155,COM6,HCI_VENDOR_EVENT,error_code,0x00,,"Indicates whether the procedure completed with an error or was successful (see ""Status error codes"" section)"
1333,13:56:46:155,COM6,HCI_VENDOR_EVENT,Raw,[0x04:0xFF:0x05:0x10:0x0C:0x01:0x08:0x00],,
1334,13:56:46:156,,HCI_VENDOR_EVENT,hci_packet_indicator,0x04,HCI Event packet,
1334,13:56:46:156,,HCI_VENDOR_EVENT,event_code,0xFF,HCI_VENDOR_EVENT,
1334,13:56:46:156,,HCI_VENDOR_EVENT,parameter_total_length,0x1B,,
1334,13:56:46:156,,HCI_VENDOR_EVENT,ecode,0x0C0E,ACI_GATT_INDICATION_EVENT,
1334,13:56:46:156,,HCI_VENDOR_EVENT,connection_handle,0x0801,,Specifies the ATT bearer for which the event applies.. Possible values:. 0x0000 ... 0x0EFF: Unenhanced ATT bearer (the parameter is the connection handle). 0xEA00 ... 0xEA3F: Enhanced ATT bearer (the LSB-byte of the parameter is the connection-oriented channel index)
1334,13:56:46:156,,HCI_VENDOR_EVENT,attribute_handle,0x0018,,The handle of the attribute
1334,13:56:46:156,,HCI_VENDOR_EVENT,attribute_value_length,0x14,,Length of Attribute_Value in octets
1334,13:56:46:156,,HCI_VENDOR_EVENT,attribute_value,0x0000000000000000000000000000000000000304,,The current value of the attribute
1334,13:56:46:156,,HCI_VENDOR_EVENT,Raw,[0x04:0xFF:0x1B:0x0E:0x0C:0x01:0x08:0x18:0x00:0x14:0x04:0x03:0x00:0x00:0x00:0x00:0x00:0x00:0x00:0x00:0x00:0x00:0x00:0x00:0x00:0x00:0x00:0x00:0x00:0x00],,
1335,13:57:16:156,,HCI_VENDOR_EVENT,hci_packet_indicator,0x04,HCI Event packet,
1335,13:57:16:156,,HCI_VENDOR_EVENT,event_code,0xFF,HCI_VENDOR_EVENT,
1335,13:57:16:156,,HCI_VENDOR_EVENT,parameter_total_length,0x04,,
1335,13:57:16:156,,HCI_VENDOR_EVENT,ecode,0x0C02,ACI_GATT_PROC_TIMEOUT_EVENT,
1335,13:57:16:156,,HCI_VENDOR_EVENT,connection_handle,0x0801,,Specifies the ATT bearer for which the event applies.. Possible values:. 0x0000 ... 0x0EFF: Unenhanced ATT bearer (the parameter is the connection handle). 0xEA00 ... 0xEA3F: Enhanced ATT bearer (the LSB-byte of the parameter is the connection-oriented channel index)
1335,13:57:16:156,,HCI_VENDOR_EVENT,Raw,[0x04:0xFF:0x04:0x02:0x0C:0x01:0x08],,
2025-12-11 1:16 AM
Thank you for the log.
Sound like being a bug in CubeMonitor-RF, because ACI_GATT_PROC_COMPLETE_EVENT happens, the tool considers the command is finished and does not wait for any further event and ignores the ACI_GATT_INDICATION_EVENT.
Issue have been reported to dev team.
2025-12-11 10:24 AM
thank you!
2026-01-23 6:42 AM
When can we expect a fixed version to be released?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.