2026-04-30 3:01 AM - last edited on 2026-04-30 3:32 AM by Andrew Neil
I have a suggestion for the STM32CubeMonitor-Power application.
For the ultra low power applications it would be great if the Y-axis could be logarithmically scaled, so that the area around 0.5-100 µA is more detailed (sleep mode) compared to the active mode (1-2 mA). As it is now I cannot quantify the current usage with a glance when the device is sleeping.
I would very much like this to be added.
Greetings,
Rico
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.