2024-03-18 6:31 AM
Hi,
I have created a project using CubeIDE 1.14.0 for the STM32L452CE. Inside the IOC editor, I changed the following things:
I then generated the code and fixed the broken linker script as outlined here: https://community.st.com/t5/stm32cubeide-mcus/stm32l452ce-cubeide-linker-script-causes-hardfault-inside-reset/m-p/651426#M25207
When I build and flash the code, I get a hardfault when executing the line:
LL_FLASH_SetLatency(LL_FLASH_LATENCY_0);
The full code is below, but it is just the default code that is generated...
/* USER CODE BEGIN Header */
/**
******************************************************************************
* @file : main.c
* @brief : Main program body
******************************************************************************
* @attention
*
* Copyright (c) 2024 STMicroelectronics.
* All rights reserved.
*
* This software is licensed under terms that can be found in the LICENSE file
* in the root directory of this software component.
* If no LICENSE file comes with this software, it is provided AS-IS.
*
******************************************************************************
*/
/* USER CODE END Header */
/* Includes ------------------------------------------------------------------*/
#include "main.h"
/* Private includes ----------------------------------------------------------*/
/* USER CODE BEGIN Includes */
/* USER CODE END Includes */
/* Private typedef -----------------------------------------------------------*/
/* USER CODE BEGIN PTD */
/* USER CODE END PTD */
/* Private define ------------------------------------------------------------*/
/* USER CODE BEGIN PD */
/* USER CODE END PD */
/* Private macro -------------------------------------------------------------*/
/* USER CODE BEGIN PM */
/* USER CODE END PM */
/* Private variables ---------------------------------------------------------*/
/* USER CODE BEGIN PV */
/* USER CODE END PV */
/* Private function prototypes -----------------------------------------------*/
void SystemClock_Config(void);
static void MX_GPIO_Init(void);
/* USER CODE BEGIN PFP */
/* USER CODE END PFP */
/* Private user code ---------------------------------------------------------*/
/* USER CODE BEGIN 0 */
/* USER CODE END 0 */
/**
* @brief The application entry point.
* @retval int
*/
int main(void)
{
/* USER CODE BEGIN 1 */
/* USER CODE END 1 */
/* MCU Configuration--------------------------------------------------------*/
/* Reset of all peripherals, Initializes the Flash interface and the Systick. */
LL_APB2_GRP1_EnableClock(LL_APB2_GRP1_PERIPH_SYSCFG);
LL_APB1_GRP1_EnableClock(LL_APB1_GRP1_PERIPH_PWR);
/* System interrupt init*/
NVIC_SetPriorityGrouping(NVIC_PRIORITYGROUP_4);
/* SysTick_IRQn interrupt configuration */
NVIC_SetPriority(SysTick_IRQn, NVIC_EncodePriority(NVIC_GetPriorityGrouping(),15, 0));
/* USER CODE BEGIN Init */
/* USER CODE END Init */
/* Configure the system clock */
SystemClock_Config();
/* USER CODE BEGIN SysInit */
/* USER CODE END SysInit */
/* Initialize all configured peripherals */
MX_GPIO_Init();
/* USER CODE BEGIN 2 */
/* USER CODE END 2 */
/* Infinite loop */
/* USER CODE BEGIN WHILE */
while (1)
{
/* USER CODE END WHILE */
/* USER CODE BEGIN 3 */
}
/* USER CODE END 3 */
}
/**
* @brief System Clock Configuration
* @retval None
*/
void SystemClock_Config(void)
{
LL_FLASH_SetLatency(LL_FLASH_LATENCY_0);
while(LL_FLASH_GetLatency()!= LL_FLASH_LATENCY_0)
{
}
LL_PWR_SetRegulVoltageScaling(LL_PWR_REGU_VOLTAGE_SCALE1);
while (LL_PWR_IsActiveFlag_VOS() != 0)
{
}
LL_RCC_MSI_Enable();
/* Wait till MSI is ready */
while(LL_RCC_MSI_IsReady() != 1)
{
}
LL_RCC_MSI_EnableRangeSelection();
LL_RCC_MSI_SetRange(LL_RCC_MSIRANGE_6);
LL_RCC_MSI_SetCalibTrimming(0);
LL_RCC_SetSysClkSource(LL_RCC_SYS_CLKSOURCE_MSI);
/* Wait till System clock is ready */
while(LL_RCC_GetSysClkSource() != LL_RCC_SYS_CLKSOURCE_STATUS_MSI)
{
}
LL_RCC_SetAHBPrescaler(LL_RCC_SYSCLK_DIV_1);
LL_RCC_SetAPB1Prescaler(LL_RCC_APB1_DIV_1);
LL_RCC_SetAPB2Prescaler(LL_RCC_APB2_DIV_1);
LL_Init1msTick(4000000);
LL_SetSystemCoreClock(4000000);
}
/**
* @brief GPIO Initialization Function
* @PAram None
* @retval None
*/
static void MX_GPIO_Init(void)
{
/* USER CODE BEGIN MX_GPIO_Init_1 */
/* USER CODE END MX_GPIO_Init_1 */
/* GPIO Ports Clock Enable */
LL_AHB2_GRP1_EnableClock(LL_AHB2_GRP1_PERIPH_GPIOA);
/* USER CODE BEGIN MX_GPIO_Init_2 */
/* USER CODE END MX_GPIO_Init_2 */
}
/* USER CODE BEGIN 4 */
/* USER CODE END 4 */
/**
* @brief This function is executed in case of error occurrence.
* @retval None
*/
void Error_Handler(void)
{
/* USER CODE BEGIN Error_Handler_Debug */
/* User can add his own implementation to report the HAL error return state */
__disable_irq();
while (1)
{
}
/* USER CODE END Error_Handler_Debug */
}
#ifdef USE_FULL_ASSERT
/**
* @brief Reports the name of the source file and the source line number
* where the assert_param error has occurred.
* @PAram file: pointer to the source file name
* @PAram line: assert_param error line source number
* @retval None
*/
void assert_failed(uint8_t *file, uint32_t line)
{
/* USER CODE BEGIN 6 */
/* User can add his own implementation to report the file name and line number,
ex: printf("Wrong parameters value: file %s on line %d\r\n", file, line) */
/* USER CODE END 6 */
}
#endif /* USE_FULL_ASSERT */
Solved! Go to Solution.
2024-03-19 4:05 AM
I ended up resolving this today - I lifted and replaced the chip with a new one, and it worked first time. So I'm going to put this one down to the ESD boogeyman I suppose. All of the flash latency modes were failing on the old one.
2024-03-18 6:42 AM
So set to using HAL only - and try.
+
>
Why this ??
2024-03-18 7:02 AM
Is there something wrong with using the LL API?
2024-03-18 7:42 AM
IF not working...seems so.
I try at first, to get something running , as it should. And HAL usually making this on the shortest time.
Playing around or improve speed is next - not first step. (Just my point of view - ymmv.)
2024-03-18 4:50 PM
I tried the HAL version, same problem. There is a hardfault at
__HAL_FLASH_SET_LATENCY(latency);
which roughly translates to the same code.
2024-03-19 1:01 AM
So - dont get me wrong: i dont "love" the HAL - use the HAL (at first) and also look, is there a update, because sometimes errors in HAL are corrected (if this is an error in HAL and not some strange setup you try to start).
(Just from thinking: you are the only one, that reports this basic error, but for sure you are not the first and only, that use this cpu; so 99% this is something in your setup (hard-and software)....)
Then begin to find out, whats wrong: without new "generate code", just writing it in actual main, set latency to ( 0-> 1 , -> 2 ) and see, what comes out; then comment out this call, to check...
And check from rm, that you have a valid setting of selected supply (smps, LDO) and core voltage and speed setting.
2024-03-19 4:05 AM
I ended up resolving this today - I lifted and replaced the chip with a new one, and it worked first time. So I'm going to put this one down to the ESD boogeyman I suppose. All of the flash latency modes were failing on the old one.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.