STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1703 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 638 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

Resolved! Installing X-CUBE-TCPP v4.0.0 in STM32CubeIDE

I have installed the example USB-C projects using the General/Import Projects from Folder or Archive option targeting the NUCELO-G474RE:DRP1M1_DRPSNK1M1_SinkSNK1M1_SourceWhat do I need to do to make these regular STM32 projects such that the Build Al...

alw by Senior
  • 2596 Views
  • 2 replies
  • 0 kudos

live expression is not opening

Hey ST, I was using cube IDE, after selecting  MCU board, we need to give project name,  while in targeted project type name i kept at  empty,  as i don't want to use IOC configuration. After successfully  writing  and debugging the code ,  if I am  ...

Sushmita by Associate II
  • 4002 Views
  • 7 replies
  • 0 kudos

Resolved! Delayed in PWM and interrupt

HiI'm implemented the most simple pwm generation and using interruptions in F401RE with TIM1. But a delay has been in the PWM generation and the update event interrupt (underflow and overflow) the most large pulse is the PWM and the another the when ...

Resolved! New STM32Project that uses Low Level drivers

STM32CubeIDE 1.12STM32G0B0RE microWe have an older Cube project from a STM32F0 series that needs to be changed to the larger STM32G0B0 chip. We thought that we would just create a new project with the new micro and port in the older code. When we cre...

0693W00000bhPzwQAE.jpg

Resolved! azure rtos on stm32h5

Hi, is there support of azure rtos for stm32h5 devices?I am looking for a MCU with ethernet and azure rtos support. I have fond some examples for sym32h7 devices but those are too big. Smallest is 100pins and they are more expensive. The smallest and...

PR.10 by Senior
  • 1941 Views
  • 1 replies
  • 0 kudos

Resolved! NetXDuo and ThreadX : Increasing number of TCP Server response

Dear Experts,I’m currently working on a project involving an STM32 board (B-U585I-IOT02A). I would like to use this board as a TCP Server . Therefore, from the STM32CUBEIDE application, I had observed that there is an example project in which it is p...

Nicolas_G_0-1708684494529.png Nicolas_G_1-1708684574247.png Nicolas_G_2-1708685721604.png
Nicolas_G by Associate II
  • 8491 Views
  • 5 replies
  • 2 kudos

I can not activate the Ethernet

Hi everyone,I have a NUCLEO-H745ZI-Q board. I try to activate ethernet, but I could not. I watched videos, read tutorials, post about it. Firstly, I thought it was my mistake. I must have made a mistake somehere, so I downloaded stm32 ethernet exampl...

code generator not work

when i try to generate "main.h" saving all after select "generate peripheral", in the window outline dont appear anything, i dont have any codei dont know how to fix it 

Manuel13_0-1710216769517.png
Manuel13 by Associate II
  • 2194 Views
  • 4 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.