2020-10-24 9:14 AM
Hello,
I bought few Blue pill modules with this MCU. But I have a problem with them in CubeIDE (Eclipse) When I try debuging or write code into MCU, there is an Error (underneath) for all modules with this MCU (STM32F103C8T6, 99lKA 98, MYS 803)
I have the same modules with CPU form different series, and there is no problem here.
A try connect this "bad" modules to CubeProgrammer and there is everything OK. I can clear Flash, write code from file, read OB and so on. I use ST LINK V2 (two pieces, the same behavior)
I try to check where the problem is, but without succes. Perharps, anybody solve this problem and could help me.
Thanks.
STMicroelectronics ST-LINK GDB server. Version 5.6.0
Copyright (c) 2020, STMicroelectronics. All rights reserved.
Starting server with the following options:
Persistent Mode : Disabled
Logging Level : 1
Listen Port Number : 61234
Status Refresh Delay : 15s
Verbose Mode : Disabled
SWD Debug : Enabled
InitWhile : Enabled
Vendor = 0x3B
Error in initializing ST-LINK device.
Reason: ST-LINK: Could not verify ST device! Abort connection.
2020-10-24 9:57 AM
Maybe your devices is in stop mode, you need add to script debug stop mode
2020-10-24 10:16 AM
How can I recognize it? I completely clear FLASH MCU a check every OB working and not working MCU. They were identical.
2020-10-24 11:09 AM
It's probably a counterfeit chip that ST-Link and/or GDB detected and decided not to communicate with.
2020-10-24 11:31 AM
It is possible. But I dont understand, why ST Programer works corectly and code is ful functional after programing by ST Programmer. When I check the protocol from ST Programmer, I notice ID
Device ID : 0x410
and gdb reported
Vendor = 0x3B
but I am not sure, that it is the same meaning.
2020-10-25 3:38 AM
Erase MCU with Programmer and try start debug with empty MCU
2020-10-25 12:45 PM
I try, but problem persist. I give it up, Perharps I buy few new MCU and rework them.
Thanks for yours advice.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.