STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1703 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 638 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

Resolved! Example project provided does not build.

Hi,I am using the above board, downloaded the example project and followed all procedure as per the readme.txt.Though I had to copy many header files into the project, I am able to create the project to 75% then it comes up with error. Please see att...

0693W000004KBE5QAO.png
Shaun.t by Associate III
  • 1445 Views
  • 2 replies
  • 0 kudos

STM32F103C8T6 problem debuging in CubeIDE

Hello,I bought few Blue pill modules with this MCU. But I have a problem with them in CubeIDE (Eclipse) When I try debuging or write code into MCU, there is an Error (underneath) for all modules with this MCU (STM32F103C8T6, 99lKA 98, MYS 803)I have...

ONadr.1 by Senior III
  • 3633 Views
  • 6 replies
  • 0 kudos

STM2 SPI state machine for HAL_BUSY

Hi,I see there are different states for SPI transfer/Receive.There are 4 different status when we use HAL_SPI_Transmit_Receive_DMA()What is the next step if we receive the status as HAL_BUSY, HAL_ERROR, HAL_TIMEOUT.Can you please help me to get some ...

Iswarya by Associate II
  • 1170 Views
  • 1 replies
  • 0 kudos

Is the CubeIDE updating thru HTTP or HTTPS?

Is the CubeIDE updating thru HTTP or HTTPS? I am using company PC, seems wont connect to http. Same problem on esp8266/Arduino https://github.com/esp8266/Arduino/issues/5480 If this is my problem, is it possible to switch the update thru https server...

Can´t update STM32CubeIDE to 1.4.2

Hello,I am trying to update my current installation (1.1.0) to 4.1.2, but CubeIDE throws this message every time.I have looked for similar problems in the forum, but seems like no one has had this issue, and I don´t know how to solve it. Anyone could...

0693W000004JzrvQAC.png
FTORR by Associate II
  • 3218 Views
  • 6 replies
  • 0 kudos

Resolved! Findout pin assignments on CubeIDE

How can I find out on a written program on CubeIDE that which pin of the microcontroller is used for different peripherals like ADC, Timer, DAC and so on?

SalPaz by Associate II
  • 7030 Views
  • 3 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.